Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How Do I Check encoder position?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How Do I Check encoder position?
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)-
      • Analog control of a Vix stepper
      • Can an Intelligent ViX-In be Programmed as a Drive
      • Configuring the ViX-drive
      • DC Brushed Motor with a ViX
      • Does the Vix have software limits?
      • Downloading Programs
      • Easi-V with Windows 7 or Windows 10
      • Homing move not complete
      • How Do I Check encoder position?
      • How to program an intelligent ViX Stepper as a Step & Direction
      • LOADENC and SCALE Commands
      • Running a Rotary Motor with a ViX-xH
      • Sample Program - Move Continuously, Stop on Inputs
      • VIX - RS232 connections
      • VIX Servo: How to Home to a Hard Stop
      • VIX Update Rates
      • ViX User Variables
      • ViX CANopen / RS-485 option
      • ViX Easi-V Error Message: Invalid data read for limits mode
      • ViX Encoder Resolution / Input Frequency
      • ViX Motor files for non-preferred BE windings
      • ViX Tuning
      • ViX servo drive Z channel encoder output
      • ViX-RJ45 RS-232 Daisy-Chain Cables
      • ViX: Connector Part Numbers
      • ViX: ViX Update Rates
      • Vix- Option 1 (MPM) Encoder Hardware Setup
      • Vix-IE with Brushed motor and Encoder
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
How Do I Check encoder position?

Print Friendly and PDF
There are several settings in the ViX that are considered to be System Variables and not commands. The actual position, PA, is one of them.

To read a system variable the syntax is: nR(xx)
where n stands for the device address and xx stands for the system variable.

For example, to read the actual position on a ViX with the address of 1, the syntax is:
1R(PA)

To set a System Variable the syntax is nW(xx,yy)
where the n stands for the device address, the xx stands for the system variable and the yy stands for the value of the variable

For example, to set the actual position to zero on a ViX with the address of 1, the syntax is:
1W(PA,0)

Some System Variable are read-only and others can be either written to or read from..

Please refer to your user guide for a list of System Variables.
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply