You need to have the HV voltage connected on the drive when you download the configuration for the drive. This is VERY important, especially if the voltage is below 80 Vdc. The drive measures the voltage and sets the current loop gains appropriately. If no HV is present, it assumes 80 Vdc.