Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Running a Rotary Motor with a ViX-xH
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Running a Rotary Motor with a ViX-xH
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)-
      • Analog control of a Vix stepper
      • Can an Intelligent ViX-In be Programmed as a Drive
      • Configuring the ViX-drive
      • DC Brushed Motor with a ViX
      • Does the Vix have software limits?
      • Downloading Programs
      • Easi-V with Windows 7 or Windows 10
      • Homing move not complete
      • How Do I Check encoder position?
      • How to program an intelligent ViX Stepper as a Step & Direction
      • LOADENC and SCALE Commands
      • Running a Rotary Motor with a ViX-xH
      • Sample Program - Move Continuously, Stop on Inputs
      • VIX - RS232 connections
      • VIX Servo: How to Home to a Hard Stop
      • VIX Update Rates
      • ViX User Variables
      • ViX CANopen / RS-485 option
      • ViX Easi-V Error Message: Invalid data read for limits mode
      • ViX Encoder Resolution / Input Frequency
      • ViX Motor files for non-preferred BE windings
      • ViX Tuning
      • ViX servo drive Z channel encoder output
      • ViX-RJ45 RS-232 Daisy-Chain Cables
      • ViX: Connector Part Numbers
      • ViX: ViX Update Rates
      • Vix- Option 1 (MPM) Encoder Hardware Setup
      • Vix-IE with Brushed motor and Encoder
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
Running a Rotary Motor with a ViX-xH

Print Friendly and PDF
It IS possible to run a rotary motor on a ViX-xH drive.

In Easi_V software, select an ViX-xE as the product that you are working with (Utilities-----> Product). Using the guided servo setup option under the Utilities menu, generate the appropriate config file.

If you need to change the resolution of the feedback, go ahead and make the changes in the file that is generated.

The firmware looks at the Resolution and max speed and determines if the resulting input frequency is above 8 MHZ (post quad) it will not accept the MOTOR command.

If the resolution is too high, then lower the max speed parameter until (Resolution x Max Velocity) / 60
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply