Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Concerns when using INH in programs
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Concerns when using INH in programs
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)-
        • Free Online Training Videos: Parker AcroBasic - Programming Basics
        • ACR7000 and ACR9000 Controller --- Interact Xpress HMI Jog Teach Sample
        • AcroBasic program does not wait
        • ACR Binary Parameter Access Examples
        • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
        • ACR Memory usage and commands
        • AcroBasic Program Priority and Timing
        • Axis Flag update rate
        • Change axis positive/negative motion direction
        • Clear all memory in an ACR controller
        • Command Syntax for Variable Substitution
        • Commenting AcroBASIC Programs
        • Concerns when using DWL in programs
        • Concerns when using INH in programs
        • Creating Watchdogs for Ethernet Connections
        • Encoder Velocity
        • Error 17000 when attempting to communicate to ACR
        • Evaluation Underflow error
        • Evaluation overflow is line xxx
        • Hardware Position Capture for Encoder 8 and 9
        • Homing Application Note for ACR7xxx/ACR9xxx Controllers and IPA Drives
        • How can I check the axis PPU setting?
        • How do I set the frequency in an ACR SINE move?
        • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
        • How fast is my servo axis moving?
        • How to Calculate the Gear Offset Parameter?
        • How to Find Torque or Current commanded from ACR
        • How to home to a limit in AcroBasic
        • How to receive ASCII data
        • How to retrieve the raw SSI position from encoder?
        • How to Simulate Motion (without drives or motors)?
        • How to use CAM ON when source is moving
        • How to use the In Motion Bit
        • INT command not working properly
        • INTCAP
        • Is the ComACRsrvr thread safe?
        • LISTEN / LRUN - How to see line numbers
        • Output on Position Toggle Mode
        • PID Parameters when using Steppers
        • Position to a Torque / Current Mode
        • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
        • prohibited names for Axis aliases
        • Range Error on download for IF ENDIF statements
        • Range Error when commanding long moves - Distance limit 2^31
        • Reboot in startup program
        • Stopping motion in ACR controllers
        • System Pointer Address of ACR Global Variables, P0-P4095
        • Use of AXIS format
        • User Variables
        • Using ACR7xxx or ACR9xxx or IPA with LabView
        • Using CAM with PPU in user units (not counts)
        • Using Encoder 8 or 9 as SRC
        • Using JOG commands with AXIS identifier
        • Using an encoder or analog input as JOG SRC
        • Variable data types and transfer to AB plc via Ethernet/IP
        • VB generates Runtime Error 91 (accessing through the ACR Comm Server)
        • What ACR Global variables should I use in HMI applications?
        • What is the Binary Host Interface
        • What is the axis velocity
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Concerns when using INH in programs

Print Friendly and PDF

The AcroBASIC inhibit command (INH) has some subtle nuances that must be known to properly use the command.

1. INH can only be used with a single flag number or alias.
2. INH cannot be used with boolean operators.
3. INH can be placed on the same line with no delimiters in between. This does not create an logical AND condition. It executes them in order from left to right, so the first condition must become true and then next INH is then evaluated. If you desire to check for multiple conditions to be true simultaneously, you must use an IF or WHILE statement.

EXAMPLES

Wait Until Active vs. Inactive:
INH 0 : REM wait until input 0 becomes active
INH -0 : REM wait until input 0 becomes inactive


This is not an AND condition:
INH 0 INH 1 INH 2 : REM Which is the same as three separate lines...
INH 0
INH 1
INH 2

To make an AND condition with IF:
IF (BIT0 AND BIT1 AND BIT2) THEN PRINT "ANDed good!"


Using an alias with INH example:
#DEFINE Moving BIT516 : REM assign an alias to bit 516
INH Moving
INH -Moving


  • Share
  • History
  • More
  • Cancel
  • Sign in to reply