Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Stopping a program
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Stopping a program
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
  • Legacy (Discontinued)-
    • 4000+
    • Compax and SV+
    • 6000+
    • APEX & APEX615x+
    • BLOK+
    • Compucam+
    • Digiplan BD, BDS, BDHX,BL, BLX,BLHX, PDS, PDX, PDHX+
    • iBE-
      • Analog Input on i-Motor
      • How many lines are on the iBE encoder?
      • i-Motor Addressing
      • i-Motor Communications
      • i-Motor I/O specs
      • i-Motor Status Byte and Word Breakdown
      • iBE minimum connections to make motion
      • iMotor and iBE Replacement
      • iMotor Downloading & Checksum
      • Keep Alive Mode
      • Max Frequency Input
      • RS485 wiring to an i-Motor
      • Stopping a program
      • Variables in i-Motors
    • 630 Family Replacement Options (631, 635, 637) (Parker SSD / Eurotherm out of Europe)
    • L20+
    • MP-FLX and FLX+
    • MPA Servo Drives+
    • Motion Architect+
    • PC21+
    • RP240+
    • S/SX Drives+
    • OEM Products+
    • SFD Servo Drives and SF Servo Motors+
    • SLVD & HPD+
    • TBF & TBN Servo Drives+
    • TQ10 & TQ10X+
    • XWare / X Language+
    • Z ZX ZXF Drives+
    • Downloading from the FTP site
    • MTS Automation / Custom Servo Motor User Guides and Documentation Location
    • Retired Products
    • Torque, Velocity & Position Loops
    • Legacy Product Page - Luge LM Series
    • Parvex Motion Explorer and Easy Rider Software
    • Running the SMA with a DC Brushed Motor
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
Stopping a program

Print Friendly and PDF
Stopping a program in an i-Motor is done by sending an END command. This does not stop motion though; that is done with the K command.

If a program is running and an END will not stop it is may be necessary to follow the below procedure.

Within the first 200 ms of power up, if the i-Motor receives a bunch of E's then it will not run the power up program. Type a bunch of E's (EEEEEEEEEEE) in the terminal, turn on the power and hit enter at the same time. This should stop the running of the power up program. Since this is time and reaction dependant it may take several attempts before the program will stop.