Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Drive Input Power
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Drive Input Power
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
  • Other-
    • -E Motor Option
    • AC-03 / AC-07 / AC-10 / AC-15 manuals
    • Battery Replacement for 500 or JSI
    • C/CX Suggested Replacements
    • Cage Code
    • Changing the Configuration of the Compumotor Plus
    • Color Code for Stepper Motor External Encoder
    • Compumotor Plus motor internal potentiometers
    • Controller Cable Drawings
    • Custom Products
    • Daedal to Compumotor Cross Reference
    • Daisy chaining AR-C
    • DC Brushed Motor with the Aries & Gemini
    • Drive Input Power
    • Dumping the 3000 memory.
    • EDC TDC XDC VRP PMC
    • Encoder or Resolver?
    • Ferrite absorber
    • Heat Dissipation within Enclosures
    • How do I change the Btorq.dat file?
    • How do I download software from www.parkermotion.com?
    • How do I get support for my Parker SSD / Parvex division products?
    • How Much Power Do I Need?
    • Inertia Ratio
    • Is Parker Compumotor ISO9000 Certified?
    • KH/KS Error 62
    • KH/KS Motors
    • M-Drive/Motor Compatibility and Matching
    • Mating MS Connectors for KH motors
    • Motion Sizer: No motor/gearhead/actuator database error (No TS torque, Divide by 0)
    • My ARC-C or -D does not fit on my motor.
    • Obsolete Products -- 1990 - 1999
    • Obsolete Products -- 2000 and later
    • Offset voltage on the Compumotor Plus
    • Parker MotionSizer: Stationary Rack, Moving Pinion
    • Parker SBC Replacement products
    • PK130M Ordering Part Number Change
    • PK2 Part Number Change(5/9/97)
    • PMC Motion Controllers (PMC20 & PMC10)
    • Printing From Compumotor DOS-based Applications
    • QM Series Motor Information
    • Refurbished Inventory / Educational Discount
    • Setting the deadband on the VAC.
    • Software for the SV
    • Three wire prox sensor color code
    • Torque Margin
    • Transformer Specs
    • Upgrading A/AX Systems
    • VM15 and VM25 Terminal Breakout Modules
    • What is a single and two speed resolver?
    • What is CE, EMC and LVD?
    • What is difference between CD35M and CD60/80M?
    • Windows 2000 locks up when printing
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
Drive Input Power

Print Friendly and PDF
To calculate the power input needed for a rotary motor use the following equation. Note you must do this for continuous and peak for servo motors (See graph below).





To calculate the power input needed for a linear motor use the following equation. Note you must do this for continuous and peak for servo motors (See graph below).






If you are sizing a DC power supply for your application, your work is nearly done. You have calculated the amount of continuous and peak power that your drive will require. If you plan to use a power supply for more than one axis, you must perform the previous steps for each axis, and you must select a power supply that will satisfy the total continuous and peak wattage for all of your axes. If you are sizing a transformer or a power supply that uses rating units of volt-amps (VA), you must now convert your requirements (in units of watts) into units of volt-amps by dividing the value in watts by a power factor of 0.66. Again, you need to consider both continuous and peak requirements for all of your axes.

IT IS IMPORTANT TO SELECT A TRANSFORMER OR POWER SUPPLY WITH A WATTAGE OR VOLT-AMP RATING THAT IS GREATER THAN THE TOTAL PEAK POWER REQUIREMENTS OF ALL YOUR AXES. IF THE RATING IS NOT GREATER, THEN YOU MUST CONSIDER USING A POWER DEVICE WITH A GREATER RATING OR YOU MUST CONSIDER USING MORE THAN ONE POWER DEVICE.



Note: The points of the torque/speed curve that are circled are the maximum power points for a servo.