Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Can I run Interact 6.X in Windows NT/2K/XP?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Can I run Interact 6.X in Windows NT/2K/XP?
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
  • Visualization and Human Machine Interface (HMI)-
    • Interact (Legacy)-
      • Replace/Upgrade Interact panel P11/P1H/P15/P2/P3/P4/P5 etc
      • CTC and i-Motors
      • Configure a TCP/IP Dial-Up Adapter Connection.
      • Interact Misc - Can ASCII register in the PLC be used as an alarm?
      • Configure a TCP/IP connection (IP address)
      • Compact Flash Disk Transfer using Interact MachineShop Toolbar to Upload and Download
      • ERROR - Invalid Panel list or Key Pad Address.
      • Ethernet download to a CTC Panel.
      • How to Restore Motion Panel.
      • Interact Software - Display alarms in a RMD tool within PTM
      • How to run app on my PowerStation on boot-up?
      • Implementing the New CMOT Driver
      • LEDs on the back of the Profibus card
      • MachineLogic - How do I clear Retentive Memory?
      • MachineLogic - No project on the PLC.
      • Security Key Setup not Installed
      • Single layer SST 5136-PFB-104 card with Interact.
      • TCP/IP Ethernet and a Dial-Up Connection
      • TCP/IP open port failure
      • Can I run Interact 6.X in Windows NT/2K/XP?
      • Can I run Interact7 on my Windows 10 or 7 PC?
      • Configure a TCP/IP connection (DHCP)
      • Configure a TCP/IP direct Ethernet connection
      • CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • Enable/disable the screen saver
      • Flashback Utilities for the CTC DOS Based PowerStations - If you have Interact ver 7 it installs all the necessary Flashbacks.
      • HMI Battery Replacements
      • How do I connect my P13, PA or PA2 Interact HMI to DataHighway Plus Network?
      • How do I recalibrate my Interact touchscreen? Or change the panel's ethernet address?
      • How do I show hidden and protected files in Windows?
      • How do I transfer my old Interact application to a newer Interact panel?
      • How to connect my device to Interact? Interact Cable Dictionary
      • How to print graphics from Interact run mode.
      • I upgraded my old hardware to a PA2 and have Vertical Stripes on screen and does not load my application.
      • Interact does not recognize the security key.
      • Interact: Error Initializing AMM - Invalid Logging Path
      • Minimum of NT 4.0 SP3 to install Machine Shop
      • Powerstation Shell on older CTC units
      • Replacing old HMIs that run Interact
      • Upgrading from a PA to a PA2
      • What are Interact Runtime modules?
      • Whats the difference between FLH-0512P and FLH-0512?
      • What internal variable can I use to R/W ASCII?
      • Interact Troubleshooting - WinXP- cannot select options on Toolbar
      • Control Access to Panels and Tools using the Password User Levels in Interact
      • Driver for my Allen Bradley Micrologix 1500 PLC?
      • Fonts and Graphics on Tools broken after Interact Upgrade to Ver 7 to run on PA2 hardware. Application runs but FONT Size or images are wrong.
      • GESNP / GESNPX 9030 / 9070 Serial Com configuration for Interact / PowerStation PA/PA2/P13 etc...
      • I need more fonts for my Interact application.
      • INTERACT How to Order
      • Interact screen size too BIG or too small after upgrade. Only see part of screen or screen compressed in top left corner of display.
      • Legacy Product Page - P1 Series
      • Legacy Product Page - P2 Series
      • Legacy Product Page - P3, P4, P5 and P7 Series
      • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
      • Security Key not found or Not programmed to support Module or Driver
      • Which HMI runs Interact?
    • InteractX+
    • Interact Xpress+
    • IXA / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (Discontinued)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • What CF Card do I need? And my HMI will not boot. Says no boot device found even after running the Flashback utility for my HMI model
    • Latest versions of HMI software packages
    • PFD - Parker Factory Display (Discontinued)+
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Can I run Interact 6.X in Windows NT/2K/XP?

Print Friendly and PDF
Only the Development software can be run in Windows NT, 2000, or XP. These versions of Window have a limited DOS shell and will not support Interact runtime with any device drivers other than the DEMO driver.
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply