Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Battery Replacement for 500 or JSI
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Battery Replacement for 500 or JSI
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
  • Other-
    • -E Motor Option
    • AC-03 / AC-07 / AC-10 / AC-15 manuals
    • Battery Replacement for 500 or JSI
    • C/CX Suggested Replacements
    • Cage Code
    • Changing the Configuration of the Compumotor Plus
    • Color Code for Stepper Motor External Encoder
    • Compumotor Plus motor internal potentiometers
    • Controller Cable Drawings
    • Custom Products
    • Daedal to Compumotor Cross Reference
    • Daisy chaining AR-C
    • DC Brushed Motor with the Aries & Gemini
    • Drive Input Power
    • Dumping the 3000 memory.
    • EDC TDC XDC VRP PMC
    • Encoder or Resolver?
    • Ferrite absorber
    • Heat Dissipation within Enclosures
    • How do I change the Btorq.dat file?
    • How do I download software from www.parkermotion.com?
    • How do I get support for my Parker SSD / Parvex division products?
    • How Much Power Do I Need?
    • Inertia Ratio
    • Is Parker Compumotor ISO9000 Certified?
    • KH/KS Error 62
    • KH/KS Motors
    • M-Drive/Motor Compatibility and Matching
    • Mating MS Connectors for KH motors
    • Motion Sizer: No motor/gearhead/actuator database error (No TS torque, Divide by 0)
    • My ARC-C or -D does not fit on my motor.
    • Obsolete Products -- 1990 - 1999
    • Obsolete Products -- 2000 and later
    • Offset voltage on the Compumotor Plus
    • Parker MotionSizer: Stationary Rack, Moving Pinion
    • Parker SBC Replacement products
    • PK130M Ordering Part Number Change
    • PK2 Part Number Change(5/9/97)
    • PMC Motion Controllers (PMC20 & PMC10)
    • Printing From Compumotor DOS-based Applications
    • QM Series Motor Information
    • Refurbished Inventory / Educational Discount
    • Setting the deadband on the VAC.
    • Smart Encoder Compatibility
    • Software for the SV
    • Three wire prox sensor color code
    • Torque Margin
    • Transformer Specs
    • Upgrading A/AX Systems
    • VM15 and VM25 Terminal Breakout Modules
    • What is a single and two speed resolver?
    • What is CE, EMC and LVD?
    • What is difference between CD35M and CD60/80M?
    • Windows 2000 locks up when printing
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
Battery Replacement for 500 or JSI

Print Friendly and PDF
1) Remove power from the unit.

2) Remove all other connectors.

3) Remove the four perimeter screws that anchor the front interface panel to the rest of the unit. Lift the front panel straight away from the unit. This will bring the circuit boards out of the unit. The battery is located on the control board, nearest the LED display.

4) Carefully remove the battery by sliding, not lifting. Be sure that the battery leaf spring has adequate tension to ensure the battery is not loose upon installation (bend down slightly).

5)Install the new battery, noting polarity. Reassemble the unit (lethal voltages present).

6) Return all connectors.

7) Apply power.

8) Establish RS-232C communications.

9a) 500 indexers: Issue the nXC command. Issue nRSE (where n is the device address of the unit). You should not get an error #30. Re-download your program. You are done.

9b) JSI controllers: Issue the nXC command. You will not be clear of the error #30 (EEPROM error) until you issue the nSV command to save all tuning etc. to non-volatile RAM. Re-download your program and issue nSV. You are done.

The replacement battery is a 3 volt lithium battery (Panasonic BR2032 or similar). These can be found at your local electronics store.