Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Using Encoder 8 or 9 as SRC
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Using Encoder 8 or 9 as SRC
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)-
        • Free Online Training Videos: Parker AcroBasic - Programming Basics
        • ACR7000 and ACR9000 Controller --- Interact Xpress HMI Jog Teach Sample
        • AcroBasic program does not wait
        • ACR Binary Parameter Access Examples
        • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
        • ACR Memory usage and commands
        • AcroBasic Program Priority and Timing
        • Axis Flag update rate
        • Change axis positive/negative motion direction
        • Clear all memory in an ACR controller
        • Command Syntax for Variable Substitution
        • Commenting AcroBASIC Programs
        • Concerns when using DWL in programs
        • Concerns when using INH in programs
        • Creating Watchdogs for Ethernet Connections
        • Encoder Velocity
        • Error 17000 when attempting to communicate to ACR
        • Evaluation Underflow error
        • Evaluation overflow is line xxx
        • Hardware Position Capture for Encoder 8 and 9
        • Homing Application Note for ACR7xxx/ACR9xxx Controllers and IPA Drives
        • How can I check the axis PPU setting?
        • How do I set the frequency in an ACR SINE move?
        • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
        • How fast is my servo axis moving?
        • How to Calculate the Gear Offset Parameter?
        • How to Find Torque or Current commanded from ACR
        • How to home to a limit in AcroBasic
        • How to receive ASCII data
        • How to retrieve the raw SSI position from encoder?
        • How to Simulate Motion (without drives or motors)?
        • How to use CAM ON when source is moving
        • How to use the In Motion Bit
        • INT command not working properly
        • INTCAP
        • Is the ComACRsrvr thread safe?
        • LISTEN / LRUN - How to see line numbers
        • Output on Position Toggle Mode
        • PID Parameters when using Steppers
        • Position to a Torque / Current Mode
        • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
        • prohibited names for Axis aliases
        • Range Error on download for IF ENDIF statements
        • Range Error when commanding long moves - Distance limit 2^31
        • Reboot in startup program
        • Stopping motion in ACR controllers
        • System Pointer Address of ACR Global Variables, P0-P4095
        • Use of AXIS format
        • User Variables
        • Using ACR7xxx or ACR9xxx or IPA with LabView
        • Using CAM with PPU in user units (not counts)
        • Using Encoder 8 or 9 as SRC
        • Using JOG commands with AXIS identifier
        • Using an encoder or analog input as JOG SRC
        • Variable data types and transfer to AB plc via Ethernet/IP
        • VB generates Runtime Error 91 (accessing through the ACR Comm Server)
        • What ACR Global variables should I use in HMI applications?
        • What is the Binary Host Interface
        • What is the axis velocity
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Using Encoder 8 or 9 as SRC

Print Friendly and PDF

Using ENC8 or ENC9 as a source (e.g. CAM SRC or GEAR SRC) on an ACR8010 or ACR8020 will cause an "OUT OF RANGE" error when using the syntax of "CAM SRC AXIS0 ENC8"

To solve this problem use the Encoder Position Register for that encoder instead.

example: CAM SRC AXIS0 P6272

Encoder Position Register (Encoder 8) - P6272
Encoder Position Register (Encoder 9) - P6288

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply