Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Motion Architect & Win98
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Motion Architect & Win98
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
  • Legacy (Discontinued)-
    • 4000+
    • Compax and SV+
    • 6000+
    • APEX & APEX615x+
    • BLOK+
    • Compucam+
    • Digiplan BD, BDS, BDHX,BL, BLX,BLHX, PDS, PDX, PDHX+
    • iBE+
    • 630 Family Replacement Options (631, 635, 637) (Parker SSD / Eurotherm out of Europe)
    • L20+
    • MP-FLX and FLX+
    • MPA Servo Drives+
    • Motion Architect-
      • AT Card DLL Drivers, WinRT and Windows Registry
      • Autobaud with Motion Architect
      • Compatibility Between DLL Files and VBasic
      • I cannot change the settings in Motion Architect.
      • Incomplete Servo Tuner Capture
      • Motion Architect & Win98
      • Multiple AT cards crashing your high-level app?
      • My Daisy Chain will not work from my Panel.
      • Not enough space for environment error
      • Reboot to start drivers error message
      • RS232 Troubleshooting for 6000 Series Products
      • Servo Tuner is returning odd data.
      • Servo Tuner not fully capturing data
      • USB-to-serial Adapters with Motion Architect
      • VIDEO: Motion Toolbox
      • VIDEO: Servo Tuner for 6000 series servo controllers (6250 & 6450)
      • WindowsNT/2000/XP compatibility.
    • PC21+
    • RP240+
    • S/SX Drives+
    • OEM Products+
    • SFD Servo Drives and SF Servo Motors+
    • SLVD & HPD+
    • TBF & TBN Servo Drives+
    • TQ10 & TQ10X+
    • XWare / X Language+
    • Z ZX ZXF Drives+
    • Downloading from the FTP site
    • MTS Automation / Custom Servo Motor User Guides and Documentation Location
    • Retired Products
    • Torque, Velocity & Position Loops
    • Legacy Product Page - Luge LM Series
    • Parvex Motion Explorer and Easy Rider Software
    • Running the SMA with a DC Brushed Motor
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
Motion Architect & Win98

Print Friendly and PDF
If you are installing Motion Architect onto Windows 98, you may encounter the error "ISINST30 caused a general protection fault......" This error is caused by a conflict between the Motion Architect installation program and a driver being used on the computer.

The driver that most commonly causes the conflict is the driver used by the Microsoft Intellipoint Mouse, MSWHEEL. Other drivers may cause the problem, but have not yet been identified.

To resolve the problem with MSWHEEL, disable the Intellipoint Mouse during the installation. To disable the mouse, press Control-Alt-Delete and end the task titled MSWHEEL. After this, begin the Motion Architect Installation again. The Intellipoint mouse will be enabled again automatically the next time you start up the computer.

If MSWHEEL is not running, the conflict is caused by a different driver. The driver in question may be identified by ending one task at a time via the Task Manager (reached by hitting Control-Alt-Delete) and restarting the Motion Architect installation process each time.

If the error still persist after all task have been ended, the problem could be a conflict with the system resources. Try disabling system resources that are not needed. For example, disable the sound, com ports, etc. This can be done by going to Start/Settings/Control Panel/System. When the System Properties are brought up, click on the Device Manager tab. Double click on the desired device and disable.

This error only happens during installation and will not occur when running Motion Architect.