The 6K program will stop execution when the power to the EVM32 is removed, even if the program is not using the inputs. This is to insure the integrity of the system; The 6K monitors this connection to make sure no cables have been cut or broken. ERROR bit 18 reports this fault.