When using the SM and N (Neo) servo motors with encoder feedback you must power both the hall and encoder 5VDC and ground. The Hall 5VDC and ground power the LEDs for the optical portion of the encoder. The encoder 5VDC and ground power the electronics portion of the encoder. Thus if either one of these is not powered the encoder will not function.
NOTE: This is done for electrical isolation purposes.