Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Problems with the EASON1000 and ZETA6104
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Problems with the EASON1000 and ZETA6104
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
  • Stepper Drives and Stepper Drive/Controller-
    • Zeta (Legacy)-
      • Stepper Motor Current Settings
      • Are the ZETA dip switches Apk or Arms?
      • Basic Setup on a ZETA61XX
      • Can Motion Architect run in Windows 7
      • Changes in Input Specifications for ZETA6104
      • Differences between OEMZL6104 and Zeta6104?
      • DRES Command
      • Getting Motion Without P-CUT Grounded
      • Maximum Cable Lengths
      • Problems with the EASON1000 and ZETA6104
      • RS485 2-wire Connection to Zeta6nnn
      • Video: How to Use Motion Architect to Upload/Download to 6000 series
      • VIDEO: Zeta6000: How to upload & download using MotionPlanner
      • What are the power req for OEM6104ZL?
      • What replaces a 87-014030-02A? Part number is ZETA4
      • What replaces a ZETA6104 or ZETA6108? OEM6104?
      • ZETA / OEMZL Family Connector Part Numbers
      • Zeta6104 Daisy Chaining Drives Together using Motion Planner
      • Zeta: Connector Part Numbers
      • Zeta: How much filtering is done internally?
    • E-Series+
    • VIX IM (Legacy)+
  • Gearheads+
  • AC/DC Industrial Drives+
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
Problems with the EASON1000 and ZETA6104

Print Friendly and PDF
When using an EASON 1000 panel to send immediate commands to a ZETA6104 while the ZETA is not running any programs, we have heard of a problem with the ZETA locking up after many cycles. The same lockup will not occur if the immediate commands are sent from Motion Architect. We have found that by setting the following modes on the ZETA the lockup will no longer occur:

ERRLVL0
ECHO0

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply