Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Why is the motor not moving when I command it to?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Why is the motor not moving when I command it to?
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
  • Legacy (Discontinued)-
    • 4000+
    • Compax and SV+
    • 6000-
      • 6000 Servo Products I/O Updates
      • 6000 Step Products Analog Inputs
      • 6250 Analog Input Option (-ANI)
      • 6250 and AT6250 Third Encoder Port
      • AT Servo Cards & Windows NT - OS Lock-Up
      • AT6000 Auxiliary Cables
      • AT6000 Product Issues
      • AT6200 and AT6400 are now CE marked
      • AT6XXX
      • AT6xxx Operating System Compatibility
      • AT6xxx Operating System Files
      • Auto-load operating system at startup
      • Backing up 6000 Programs
      • Bad DLL Calling Convention
      • Control Velocity with an Analog Input.
      • DDE 6000 and Excel
      • Downloading Programs in a Daisy Chain
      • Home Backup Controls Cluster with Motion Toolbox
      • Homing to Z channel on 6000 products
      • HOMLVL command
      • How do I change velocity on the fly during JOGGING?
      • How do I make a program run on power up?
      • How do I make a proper back up for my 6000 series controller?
      • How to send/receive with OCX
      • Input Buffer for 6000 Serial Producs
      • Input Debounce Times for 6000 Series Products
      • Input Impedance for -ANI option for AT6n50
      • Interrupts, AT cards & troubleshooting
      • Linker Error
      • LSCW and LSPOS are the same command
      • Minimum files for AT card
      • Model 6201 Information
      • Motion Architect and WinRT
      • Motion Toolbox in a Daisy Chain
      • PCOMP in Conditional Statements
      • Reading in multiple numbers with the TM8
      • ReceiveFile method bug
      • RecvAT6400Block documentation error
      • Running more than 199 programs in 6000 Products
      • Scaling With the 6000 Products
      • Sequence Names Can Cause Problems.
      • SetNTMultiCardAddress doc error
      • Status Bits and Commanding a Velocity of Zero
      • Unable to get Procaddress32W for wrtoutpw error
      • VIDEO: DDE Server - Communicating from MS-Excel
      • Visual Basic Sample with AT Card
      • What addresses are in use on my NT machine?
      • What can I use as a replacement for my 6200 or OEM6200 indexer?
      • What can I use as a replacement for my 6250 or OEM6250 servo controller?
      • What can I use as a replacement for my AT6200 or AT6400 indexer?
      • What can I use as a replacement for my AT6250 or AT6450 servo controller?
      • What is WinRT anyway?
      • Why does RESET6000.VI cause error 5004 in Labview?
      • Why is my AT-card locking up?
      • Why is the motor not moving when I command it to?
      • X language to 6000 series language
    • APEX & APEX615x+
    • BLOK+
    • Compucam+
    • Digiplan BD, BDS, BDHX,BL, BLX,BLHX, PDS, PDX, PDHX+
    • iBE+
    • 630 Family Replacement Options (631, 635, 637) (Parker SSD / Eurotherm out of Europe)
    • L20+
    • MP-FLX and FLX+
    • MPA Servo Drives+
    • Motion Architect+
    • PC21+
    • RP240+
    • S/SX Drives+
    • OEM Products+
    • SFD Servo Drives and SF Servo Motors+
    • SLVD & HPD+
    • TBF & TBN Servo Drives+
    • TQ10 & TQ10X+
    • XWare / X Language+
    • Z ZX ZXF Drives+
    • Downloading from the FTP site
    • MTS Automation / Custom Servo Motor User Guides and Documentation Location
    • Retired Products
    • Torque, Velocity & Position Loops
    • Legacy Product Page - Luge LM Series
    • Parvex Motion Explorer and Easy Rider Software
    • Running the SMA with a DC Brushed Motor
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
Why is the motor not moving when I command it to?

Print Friendly and PDF
If the Controller and Drive are separate units, make sure the DRFLVL is set correctly. Also make sure that the drive is enabled with the DRIVE command. If they are in the same unit (APEX615n and ZETA61XX units), then the DRFLVL command is invalid.

Servos: make sure that the Enable (ENBL) pin is grounded.

Steppers: make sure that the P-CUT pin is grounded.

Type the command TASF. This command provides good information about the status of the controller.

Are either bits 17 or 18 on TAS high?
YES: A hard limit is hit.

Are Hard Limits being used?
YES: Check to see if the load is at a limit; if it is not, then check to make sure the wiring is correct.
NO: Disable the Hard Limits with the LH command.