Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Establishing Communication with the PDX
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Establishing Communication with the PDX
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
  • AC/DC Industrial Drives+
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
  • Legacy (Discontinued)-
    • 4000+
    • Compax and SV+
    • 6000+
    • APEX & APEX615x+
    • BLOK+
    • Compucam+
    • Digiplan BD, BDS, BDHX,BL, BLX,BLHX, PDS, PDX, PDHX-
      • Battery for the PDX &TQ10X Drive
      • Battery Replacement for BDHX,BLX,BLHX,PDHX, X150
      • BL, BLX, BLH, BLHX, ML Suggested Replacements
      • BLHX Error
      • BLHX Error #25
      • BLHX Part Number
      • BLHX Registration Speed
      • BLX Outputs.
      • Can I use a ML motor in place of a MD motor?
      • Error code 3 - Memory map changed
      • Establishing Communication with the PDX
      • No Communication with the BDHX?
      • No motion? Check motor resolution for the PDX
      • PDHX-E Troubleshooting Codes.
      • PDHX15E Self Test
      • PDS Power Dump Option(-D)
      • PDS Replacement
      • PDS13 PDS15 PDX13 PDX15 Connector Part Numbers
      • PDX Replacement
      • Removal of RS485 in PDHX-E and BDHX-E
    • iBE+
    • 630 Family Replacement Options (631, 635, 637, 638) (Parker SSD / Eurotherm out of Europe)
    • L20+
    • MP-FLX and FLX+
    • MPA Servo Drives+
    • Motion Architect+
    • PC21+
    • RP240+
    • S/SX Drives+
    • OEM Products+
    • SFD Servo Drives and SF Servo Motors+
    • SLVD & HPD+
    • TBF & TBN Servo Drives+
    • TQ10 & TQ10X+
    • XWare / X Language+
    • Z ZX ZXF Drives+
    • Downloading from the FTP site
    • MTS Automation / Custom Servo Motor User Guides and Documentation Location
    • Retired Products
    • Torque, Velocity & Position Loops
    • Legacy Product Page - Luge LM Series
    • Parvex Motion Explorer and Easy Rider Software
    • Running the SMA with a DC Brushed Motor
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
Establishing Communication with the PDX

Print Friendly and PDF
Here are two important tips that will help you establish communication with the PDX. After you have connected in terminal mode using X-ware, you will notice that you do not see a prompt ">" like some of the other x-ware products. This is normal. The PDX does not return a prompt at the terminal.

In order to verify your communication with PDX you need to know that the default address for the PDX is 8. Unlike some the other X products which default to 1, the PDX has three hardware address select inputs on the 25 pin connector which if left untouched result in a address of 8. In order to get a response from the unit you must precede the command with a valid device address. One of the best commands to help determine a devices address is the R command. Issuing 8R(be sure to use capital letters) should give you a response of *R, *S,*B , *C . If you do not see a response to this, the unit may have been set to a different address in which case you will need to try a different address with the R command, like 1R,2R, 3R until you receive a response.
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply