Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Scaling With the 6000 Products
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Scaling With the 6000 Products
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
  • Legacy (Discontinued)-
    • 4000+
    • Compax and SV+
    • 6000-
      • 6000 Servo Products I/O Updates
      • 6000 Step Products Analog Inputs
      • 6250 Analog Input Option (-ANI)
      • 6250 and AT6250 Third Encoder Port
      • AT Servo Cards & Windows NT - OS Lock-Up
      • AT6000 Auxiliary Cables
      • AT6000 Product Issues
      • AT6200 and AT6400 are now CE marked
      • AT6XXX
      • AT6xxx Operating System Compatibility
      • AT6xxx Operating System Files
      • Auto-load operating system at startup
      • Backing up 6000 Programs
      • Bad DLL Calling Convention
      • Control Velocity with an Analog Input.
      • DDE 6000 and Excel
      • Downloading Programs in a Daisy Chain
      • Home Backup Controls Cluster with Motion Toolbox
      • Homing to Z channel on 6000 products
      • HOMLVL command
      • How do I change velocity on the fly during JOGGING?
      • How do I make a program run on power up?
      • How do I make a proper back up for my 6000 series controller?
      • How to send/receive with OCX
      • Input Buffer for 6000 Serial Producs
      • Input Debounce Times for 6000 Series Products
      • Input Impedance for -ANI option for AT6n50
      • Interrupts, AT cards & troubleshooting
      • Linker Error
      • LSCW and LSPOS are the same command
      • Minimum files for AT card
      • Model 6201 Information
      • Motion Architect and WinRT
      • Motion Toolbox in a Daisy Chain
      • PCOMP in Conditional Statements
      • Reading in multiple numbers with the TM8
      • ReceiveFile method bug
      • RecvAT6400Block documentation error
      • Running more than 199 programs in 6000 Products
      • Scaling With the 6000 Products
      • Sequence Names Can Cause Problems.
      • SetNTMultiCardAddress doc error
      • Status Bits and Commanding a Velocity of Zero
      • Unable to get Procaddress32W for wrtoutpw error
      • VIDEO: DDE Server - Communicating from MS-Excel
      • Visual Basic Sample with AT Card
      • What addresses are in use on my NT machine?
      • What can I use as a replacement for my 6200 or OEM6200 indexer?
      • What can I use as a replacement for my 6250 or OEM6250 servo controller?
      • What can I use as a replacement for my AT6200 or AT6400 indexer?
      • What can I use as a replacement for my AT6250 or AT6450 servo controller?
      • What is WinRT anyway?
      • Why does RESET6000.VI cause error 5004 in Labview?
      • Why is my AT-card locking up?
      • Why is the motor not moving when I command it to?
      • X language to 6000 series language
    • APEX & APEX615x+
    • BLOK+
    • Compucam+
    • Digiplan BD, BDS, BDHX,BL, BLX,BLHX, PDS, PDX, PDHX+
    • iBE+
    • 630 Family Replacement Options (631, 635, 637) (Parker SSD / Eurotherm out of Europe)
    • L20+
    • MP-FLX and FLX+
    • MPA Servo Drives+
    • Motion Architect+
    • PC21+
    • RP240+
    • S/SX Drives+
    • OEM Products+
    • SFD Servo Drives and SF Servo Motors+
    • SLVD & HPD+
    • TBF & TBN Servo Drives+
    • TQ10 & TQ10X+
    • XWare / X Language+
    • Z ZX ZXF Drives+
    • Downloading from the FTP site
    • MTS Automation / Custom Servo Motor User Guides and Documentation Location
    • Retired Products
    • Torque, Velocity & Position Loops
    • Legacy Product Page - Luge LM Series
    • Parvex Motion Explorer and Easy Rider Software
    • Running the SMA with a DC Brushed Motor
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
Scaling With the 6000 Products

Print Friendly and PDF

If you are having problems with scaling in the 6000 products, the most common cause is not having the scaling factors both inside and outside of your start up program. The one rule about scaling to remember is that the scale factors need to be set both in the program and also set when the program is downloaded. By placing the scale factors before the DEL and DEF, this will insure the factors will get set on the download. This is because any commands outside of DEF and END are executed when you download.

Below is an example of what your program should look like in the Editor.

SCLA50000,50000
SCLV50000,50000
SCLD50000,50000
SCALE1

DEL SETUP
DEF SETUP

SCLA50000,50000
SCLV50000,50000
SCLD50000,50000
SCALE1

A10,10
V5,5
D3,3
GO11

END
STARTP SETUP


*When using Motion Planner with the Zeta controller, you will need to download the program twice for the new scaling parameters to take effect. Alternatively, you can enter the scaling into the terminal window directly for them to take effect.  Motion Architect is the software package designed to work with the Zeta controller and scaling is handled differently when using Motion Planner with Zeta.

updated 1 Apr 2015 nc