Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Getting Motion Without P-CUT Grounded
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Getting Motion Without P-CUT Grounded
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
  • Stepper Drives and Stepper Drive/Controller-
    • Zeta (Legacy)-
      • Stepper Motor Current Settings
      • Are the ZETA dip switches Apk or Arms?
      • Basic Setup on a ZETA61XX
      • Can Motion Architect run in Windows 7
      • Changes in Input Specifications for ZETA6104
      • Differences between OEMZL6104 and Zeta6104?
      • DRES Command
      • Getting Motion Without P-CUT Grounded
      • Maximum Cable Lengths
      • Problems with the EASON1000 and ZETA6104
      • RS485 2-wire Connection to Zeta6nnn
      • Video: How to Use Motion Architect to Upload/Download to 6000 series
      • VIDEO: Zeta6000: How to upload & download using MotionPlanner
      • What are the power req for OEM6104ZL?
      • What replaces a 87-014030-02A? Part number is ZETA4
      • What replaces a ZETA6104 or ZETA6108? OEM6104?
      • ZETA / OEMZL Family Connector Part Numbers
      • Zeta6104 Daisy Chaining Drives Together using Motion Planner
      • Zeta: Connector Part Numbers
      • Zeta: How much filtering is done internally?
    • E-Series+
    • VIX IM (Legacy)+
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
Getting Motion Without P-CUT Grounded

Print Friendly and PDF
P-CUT was designed as a safety connection. The idea is that P-CUT needs to be grounded in order for the ZETA to produce motion (#1 below).

With the addition of the V_I/O pin in October of 1997, there is one stipulation in order for the P-CUT to stop motion when disconnected from GND: V_I/O must be pulled up.

If the V_I/O pin is not pulled up to either +5V or +24V, then motion may be produced regardless of whether the P-CUT is grounded or not (#2 and #3 below).

If the AUX-P pin is not pulled up (it is either grounded or not connected), then the V_I/O needs to be pulled up in order for the P-CUT to be able to stop motion. This time, the P-CUT must be connected to +5V to stop the motion. As long as the P-CUT is not pulled up (either it is grounded or not connected), then motion may occur (#4 and #5 below).


P-CUTAUX-PV_I/OMOTION
1GNDXXYes
2openXopenYes
3openX+5VNo
4openopen+5VYes
5+5Vopen+5VNo


X = does not matter
open = no connection
GND = connected to Ground
+5V = connected to either 5 VDC or 24 VDC