Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Manual Alignment Procedure
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Manual Alignment Procedure
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)-
      • Controller (CE)+
      • Drive only (AE,AR, SE, SR)+
      • EPL+
      • AR-20 and AR-30 minimum AC voltage
      • Absolute Encoders & Drive Compatibility
      • Aries - MaxPlus (MPM) Encoder Option 1 Connection
      • Aries - MaxPlus (MPM) Resolver Option 1 Connection
      • Aries Brake Delay
      • Aries Drive: Connector Part Numbers
      • Bayside GM Gearmotor Files for Aries
      • Cables to connect GM motors to Parker Drives
      • Can I use Aries drives with MX80L linear motor stages?
      • DTALK with Aries 3.32 & higher firmware
      • E27 Bridge Hardware Fault
      • E54 Feedback Loss Fault - 5 Green Flash 1 Yellow
      • How do I power an ARIES with 3 phase?
      • How do I know Aries SFB is set to auto-detect?
      • How to Update Operating System (Firmware)
      • Manual Alignment Procedure
      • Peak Current Time from Compumotor Drives
      • Aries drive won't enable
      • Selecting a Fuse
      • Using R100,R150 and R200 with Aries
      • Aries (AR-xxAE or AR-xxSE) Recommended Replacements
      • Aries 2000/3000 watt Replacements (AR-20AE, AR-30AE, AR-20SE, AR-30SE)
      • Aries Resolver Replacement (AR-01AR, AR-02AR, AR-04AR, AR-08AR, AR-13AR, AR-01SR, AR-02SR, AR-04SR, AR-08SR, AR-13SR)
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Manual Alignment Procedure

Print Friendly and PDF
For using non-Parker motors with the Aries drives, if you do not know the motor, hall and encoder phasing or are not sure, you can use the below manual alignment procedures to determine the proper motor and hall wiring.

Aries AR-xxAE or AR-xxSE Manual Alignment

AriesEPL AR-xxPE Manual Alignment

AriesController AR-xxCE Manual Alignment


For an Aries ARxx-AE with an ACR9000, to turn on the hardware enable output use these commands in the terminal:
DRIVE OFF AXIS0
CLR 8468 ;This disables Drive I/O
REN AXIS0 ;This resets the commanded position to the encoder position.
SET 40 ;This forces on Drive Enable Output 0.

Then the above Alignment Procedure can be done.
After, type in the terminal:
CLR 40 ;This disables the Drive Enable Output 0.
SET 8468 ;This enables Drive I/O.

On enable from the ACR9000 the encoder position is reset.
For other axis add 32 to 8468 and add 1 to 40. ie, Axis1 would be 8500 for Drive I/O, 41 for Drive Enable output.
For Axis3, 8564 and 43.
DRIVE ON AXIS3
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply