Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Position to a Torque / Current Mode
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Position to a Torque / Current Mode
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
  • -Motion and Machine Controllers
    • -ACR Controllers
      • +7000
      • +9000 (Legacy)
      • +IEC PLC (9600) (Legacy)
      • +PC Card Controllers (Discontinued)
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • +PAC120
    • +PAC340
    • +PAC320 (Discontinued)
    • +6K (Discontinued)
  • +General Technology Information
  • +Virtual Engineer
  • +Visualization and Human Machine Interface (HMI)
  • +Servo Drives and Servo Drive/Controllers
  • +Stepper Drives and Stepper Drive/Controller
  • +Gearheads
  • +AC and DC Drives and Inverters
  • +Servo Motors
  • +Step Motors
  • +Linear and Rotary Positioners
  • +Electric Cylinders
  • +T-Slot Aluminum Framing
  • +C3 + Xpress + ETH
  • How can I stay updated on Parker electromechanical and drives product news?
  • +Legacy (Discontinued)
  • +Other
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
  • What replaces the Gemini GV6K servo drive controller?

You are currently reviewing an older revision of this page.

  • History View current version

Position to a Torque / Current Mode

To home, position, or press/push/pull to a given torque/force using an ACR controller a few simple steps must be taken to allow for a larger position error than would be typical in a strictly position controlled system. The idea is that the maximum torque will be limited to the desired magnitude, and then a move is commanded beyond the point of expected force limit. E.G. to home to a hard stop that is 1” away, a move of 1.25” is commanded to insure that the torque limit is met.

To accomplish this:

Set the Excess Position Error “EXC” to a sufficiently large value. If the EXC window is too small, the drive will fault due to position error.

Set the axis Torque Limit “TLM” to the desired SCALED value. The TLM is scaled linearly from 0 to +/-10 V; 10V being the peak torque.

Command a move that is farther than point of resistance.

Wait for motion to stop using an Inhibit command “INH”

Optional:

Command a move that is the difference between commanded position and actual position (where motion stopped due to physical obstruction and torque limit)

X/((P12290 -P12289)/PPU Value)

Follow with a RES X to zero this location.

EXC X 3 : REM Set the Excess position Error to 3 inches
TLM X 1.5 : REM Limit torque output to 15% of maximum
X/-2
INH -516 : REM Wait for Motion to stop
X/((P12290 -P12289)/4000) : REM Command a move to the point motion stopped
RES X : REM Zero position
For Aries-EPL or AriesCE.
It is possible to put the drive into a "torque" mode by setting all tuning gains to zero and then sending TRQOFF commands to the drive to control the torque offset. This effectively runs the drive open loop, although it is necessary to tell the controller to disregard position errors by clearing the "Enable EXC Response" control flag (bit 8469 for Axis0). Note that disabling this fault could cause servo run-away. ie, If doing a clamping operation, it'd be recommended to set EXC to a value just past the clamping position.

In a sample for Axis0, set up as EPLD0, it can be as simple as:

AXIS0 PGAIN 0
AXIS0 DGAIN 0
AXIS0 IGAIN 0
AXIS0 ILIMIT 0
AXIS0 FBVEL 0
AXIS0 FFVEL 0
AXIS0 FFACC 0

For EPL:
OPEN "EPLD0:" AS #3 : REM open a channel to EPLD drive 0 as device #3
PRINT #3, "TRQOFF 1" : REM set torque offset in % of DMTLIM for EPLD0 via device #3
CLOSE #3 : REM close channel to EPLD drive 0

For AriesCE:
C164 is the torque offset and is a % of the DMTLIM. Range is -100% to +100% and is Floating Point data type.
C14 is the drive's motor torque limit (DMTLIM), can range from 0 to 4000 and is Nm for rotary or N for linear and is Floating Point data type.