Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Upload Absolute Position from a C3 to a ACR9000
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Upload Absolute Position from a C3 to a ACR9000
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • 9000 (Legacy)-
        • ACR9000 Family Letter of Volatility
        • ACR Gantry Lock and EPL Axes
        • ACR Homing Success/Failure Flags
        • ACR Order Code
        • ACR Servo Tuner - Move Back & Forth sample code
        • ACR-View 6 is frozen. How do I recover?
        • ACR-View Memory Dimensioning using the Oscilloscope
        • ACR9000 to ModuFlex connection pinout
        • Automating the EPL startup procedure
        • Can I use tools from ACR-View in my own PC application?
        • Compax3 and Aries Ethernet PowerLink I/O
        • Configuring Memory for ACR9000 Com Channels
        • Dual Loop with Analog Position Feedback
        • EPL Drive Enable Status
        • Free Online Training Videos: Parker ACR9000 programmable motion controller
        • Having problems connecting with USB - ACR View 6.0
        • How do I add PBOOT to PLC programs?
        • How much memory does my ACR controller have?
        • How to Read Compax3 Analog I/O with EPL SDO read?
        • How to connect ACR to PIO CANopen buscoupler?
        • How to disable RS232 autobaud for ACR9xxx
        • How to get status values from an Aries EPL Drive
        • How to read the absolute position from EPL drive?
        • How to select user units and axis scaling
        • INTCAP and MSEEK with Compax3 EPL
        • MSEEK EthernetPowerlink Compatibility
        • Memory Allocation for PLC programs
        • Output Reaction to EPL Failure
        • Remap CAN I/O for use with PLC
        • What is needed with various Parker I/Os?
        • What verison of the .Net Framework is needed for ACR-View 6?
        • Whats the difference between PIO-337 and PIO-347?
        • Where does ACR-View install the ComACRserver?
        • Why is controller reporting Program Stuck
        • 9000: Connector Part Numbers
        • ACR 9000 replacement: New ACR7000 series controller
        • ACR 9xx0 Recovering from Estop / Motion Enable input
        • ACR-View: Mapping a parameter to an oscilloscope channel
        • ACR9000 - CIP Communications stop on all devices when one CIP device goes offline
        • ACR9000 Ethernet Stream Connection Status Sample
        • ACR9000 Event Counters
        • ACR9000 Sample Input/Output Wiring
        • Are Parker IO modules available as NPN?
        • Connecting a Parker IO (PIO) to an ACR9000
        • EPL Velocity p38145 vs p8193 Master Velocity
        • Ethernet Communication Streams
        • Ethernet/IP Encoders
        • How do I set up Parker I/O (PIO)
        • How to command a home operation from HMI or PC app
        • Master Encoder for C3 EPL & ACR9040 system
        • Maximum USB Cable Length
        • Replacing the ACR9000 Battery
        • RS232 Electrical Noise on older 9000 Controllers
        • Senary Axis Flags
        • Updated EPL Network Flags and Parameters
        • Upload Absolute Position from a C3 to a ACR9000
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
Upload Absolute Position from a C3 to a ACR9000

Print Friendly and PDF
If you were using a Compax3 I10T10, an ACR9000 and a motor with an absolute encoder, it would be beneficial to get the absolute position from the encoder to the ACR9000. This would eliminate the need to home the system, which is most of the reason for an absolute encoder. This can be done since the ACR9000 has an RS485 output on every Axis connector that can be used for any communications and the Compax3 has a RS485 port. Follow the sections below for the details on the Cabling, Compax3 Setup and the ACR9000 Setup.

Cabling

71-021108-XX ACR to Compax3 cable, where XX is your length in feet
71-021609-01 ACR axis/communications breakout (Aries Dongle)

The above cables will provide you with one ACR9000 connection, a RS485 9 pin connector and 2 connections at the Compax3 drive. Both units' should have the same ground reference with the back of the Compax3 and ACR9000 installed to the same bare metal cabinet (not painted) or if in separate cabinets, their grounds should be tied together with a large braided shielded wire, as short as possible. At this point all the connections are made to make motion from the ACR9000 to the Compax3. The only thing left is a communications cable between the two.

ACR9000 to Compax3 Communication Cable
71-021609-01 9-Pin D-Sub Pin # Compax3 X10 Pin # Function
2 7 RS485 +
3 3 RS485 -
5 5 Ground

Connect Pins 1 and 9 on the Compax3 X10 connector to enable RS485 on the Compax3.
Compax3 Setup

After configuring the motor you will need to setup the RS485 objects.

810.1 is the RS485 Protocol (Use 16 for 2 wire setup)
810.2 is the RS485 Baud Rate
810.3 is the RS485 Node Address

These can be set from the Optimization screen in the Servomanager software or from an ASCII terminal. See the FAQ "Accessing Objects from RS232 and RS485" for more details on setting objects.

Set 810.1 = 16, 810.2 = 9600, 19200 or 38400 and finally set the node address to some number between 1 and 97. Make sure to write these values to the flash by pressing the "WF" button in the Optimization screen or writing a non-zero number to the 20.11 object.

ACR9000 Setup

With all the Cabling and Compax3 Setup complete, you should now be able to open the comm port on the ACR9000 and talk to the Compax3. This is done in 4 simple steps.

1) Type 'OPEN "COM2:nnnn,N,8,1" AS #1' where nnnn is the baud rate set on the RS485 Baud rate object of the Compax3.
If using the ACR9000's 9pin com port it would be COM1; this 9pin is RS485 4wire.

2) Using Hyperterminal, type 'TALKTO #1' This will start an interface directly to the Compax3 from the ACR9000 terminal. Do not use ACR-View for this step. TALKTO in ACR-View will not connect; user Windows Hyperterminal.

3) Type 'no680.5' where n is the RS485 address number on the Compax3, and hit enter. This should return the value of the actual position of the motor. If there is no response, make sure the Compax3 is powered as well as the Cabling and RS485 settings are correct.

4) Hit the escape key to exit this mode.
Finally to automate the process the below code should be implemented on power up to get the actual position and reset the position counters in the ACR9000 to the absolute number.

DIM DV(1)
DIM $V(10,80)
OPEN "COM2:9600,N,8,1" AS #1
DWL 0.5
$V0 = "1o680.5" + CHR$(13)
PRINT #1, $V0;
INPUT; #1, $V1
CLOSE #1
$V1 = MID$($V1,2,LEN($V1)-2)
DV0 = VAL($V1)
RES Z(DV0)

Please note that the actual position from the Compax3 drive will return in revolutions of the motor. You may need to scale this number to get the desired units for the application.