Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base What is needed with various Parker I/Os?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base What is needed with various Parker I/Os?
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
  • -Motion and Machine Controllers
    • -ACR Controllers
      • +7000
      • -9000 (Legacy)
        • ACR9000 Family Letter of Volatility
        • ACR Gantry Lock and EPL Axes
        • ACR Homing Success/Failure Flags
        • ACR Order Code
        • ACR Servo Tuner - Move Back & Forth sample code
        • ACR-View 6 is frozen. How do I recover?
        • ACR-View Memory Dimensioning using the Oscilloscope
        • ACR9000 to ModuFlex connection pinout
        • Automating the EPL startup procedure
        • Can I use tools from ACR-View in my own PC application?
        • Compax3 and Aries Ethernet PowerLink I/O
        • Configuring Memory for ACR9000 Com Channels
        • Dual Loop with Analog Position Feedback
        • EPL Drive Enable Status
        • Free Online Training Videos: Parker ACR9000 programmable motion controller
        • Having problems connecting with USB - ACR View 6.0
        • How do I add PBOOT to PLC programs?
        • How much memory does my ACR controller have?
        • How to Read Compax3 Analog I/O with EPL SDO read?
        • How to connect ACR to PIO CANopen buscoupler?
        • How to disable RS232 autobaud for ACR9xxx
        • How to get status values from an Aries EPL Drive
        • How to read the absolute position from EPL drive?
        • How to select user units and axis scaling
        • INTCAP and MSEEK with Compax3 EPL
        • MSEEK EthernetPowerlink Compatibility
        • Memory Allocation for PLC programs
        • Output Reaction to EPL Failure
        • Remap CAN I/O for use with PLC
        • What is needed with various Parker I/Os?
        • What verison of the .Net Framework is needed for ACR-View 6?
        • Whats the difference between PIO-337 and PIO-347?
        • Where does ACR-View install the ComACRserver?
        • Why is controller reporting Program Stuck
        • 9000: Connector Part Numbers
        • ACR 9000 replacement: New ACR7000 series controller
        • ACR 9xx0 Recovering from Estop / Motion Enable input
        • ACR-View: Mapping a parameter to an oscilloscope channel
        • ACR9000 - CIP Communications stop on all devices when one CIP device goes offline
        • ACR9000 Ethernet Stream Connection Status Sample
        • ACR9000 Event Counters
        • ACR9000 Sample Input/Output Wiring
        • Are Parker IO modules available as NPN?
        • Connecting a Parker IO (PIO) to an ACR9000
        • EPL Velocity p38145 vs p8193 Master Velocity
        • Ethernet Communication Streams
        • Ethernet/IP Encoders
        • How do I set up Parker I/O (PIO)
        • How to command a home operation from HMI or PC app
        • Master Encoder for C3 EPL & ACR9040 system
        • Maximum USB Cable Length
        • Replacing the ACR9000 Battery
        • RS232 Electrical Noise on older 9000 Controllers
        • Senary Axis Flags
        • Updated EPL Network Flags and Parameters
        • Upload Absolute Position from a C3 to a ACR9000
      • +IEC PLC (9600) (Legacy)
      • +PC Card Controllers (Discontinued)
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • +PAC120
    • +PAC340
    • +PAC320 (Discontinued)
    • +6K (Discontinued)
  • +General Technology Information
  • +Virtual Engineer
  • +Visualization and Human Machine Interface (HMI)
  • +Servo Drives and Servo Drive/Controllers
  • +Stepper Drives and Stepper Drive/Controller
  • +Gearheads
  • +AC and DC Drives and Inverters
  • +Servo Motors
  • +Step Motors
  • +Linear and Rotary Positioners
  • +Electric Cylinders
  • +T-Slot Aluminum Framing
  • +C3 + Xpress + ETH
  • How can I stay updated on Parker electromechanical and drives product news?
  • +Legacy (Discontinued)
  • +Other
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
  • What replaces the Gemini GV6K servo drive controller?

You are currently reviewing an older revision of this page.

  • History View current version

What is needed with various Parker I/Os?

CONNECTING POWER TO BUS COUPLER
When using a PIO337, there are two separate connections for 24VDC supplies. The “24V” and “0V” provides the logic power for the CANopen bus coupler and the I/O modules. The two “+” and two “-“ connections provide the “field power” or “bus power” for the modules, this provides the 24VDC I/O power for devices connected to the digital I/O modules.

When using the PIO347, only a single power connection is available and that is for the logic supply. To connect the bus power, a PIO 602 will also need to be used in conjunction with Digital I/Os. If you are using a 2- or 4-input digital input or output module, then you can land the 24V bus power on the middle terminals. The 24V connection would go to connectors 2 or 6, the 0V or “24V RTN” connection would go to connectors 3 or 7.

CONNECTING I/O MODULES TO BUS COUPLER
Placement of the I/O modules matters greatly due to the “power contacts” on the sides of some of the I/O modules. There are blade contacts and spring contacts on the digital modules to pass the 24VDC field bus power to the next unit. Since the analog modules do not need the 24VDC for their operation they do not have these contacts. Some units have three contacts of each, some have two contacts of each, others have no contacts. Refer to the appropriate bus coupler documentation for installation information.
We recommend placing digitals I/O modules closest to the bus coupler then the Analog I/O modules. Modules may be placed in any configuration, but either a PIO602 or 24VDC will be needed to provide BUS voltage to the rest of the Digital I/Os.

TERMINATION MODULES
Both the PIO337 and the PIO347 need a PIO600 termination module.

SETTING BAUD RATE
Please refer to page 40 of the CAN_STD_PIO-337.pdf or page 33 of the CAN_ECO_PIO-347.pdf which are located on the webpage: http://www.parkermotion.com/manuals/PIO/PIO.html.

SETTING BUS COUPLER ADDRESS (MODULE ID)
Please refer to page 39 of the CAN_STD_PIO-337.pdf or page 33 of the CAN_ECO_PIO-347.pdf which are located on the webpage: http://www.parkermotion.com/manuals/PIO/PIO.html.