Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base TASX Bit 10 - Bridge Fault (Hardware)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base TASX Bit 10 - Bridge Fault (Hardware)
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)-
      • 24 Volt Keep Alive
      • Analog input on GV6, GV6K, GT6, GT6K
      • Audible Noise in Stepper Motors
      • Cable breakout modules for the Gemini
      • Can I run the MX80L using a Gemini Drive?
      • Can the Gemini Products take a DC voltage supply?
      • Changing Motor direction on the GV6 or GT6
      • Chopping frequency of the Gemini drive.
      • Connector Part Numbers
      • Controller to GV Cables
      • Currently Released Gemini Drive Products
      • Daisy chaining GVs and GTs
      • Digital Notch Filters
      • Does the Gemini drive have a test mode?
      • Downloading the OS to my Gem6K locks up.
      • Encoder Motors Work with Gemini Resolver units
      • ERES /ORES Relationship for Gemini GV Products
      • GC-SDA Fault output is not really the fault output
      • GEM-VM50 screw-terminal breakout dimensions
      • Gem6K (GV6K & GT6K) Family Letter of Volatility
      • Gemini MaxPlus (MPM) Resolver Option 1 Connection
      • Gemini - Downloading in
      • Gemini - MaxPlus (MPM) Encoder Option 1 Connection
      • Gemini - MaxPlus (MPM) Encoder Option 5 Connection
      • Gemini Analog Input Deadband
      • Gemini Analog Output A now dithers
      • Gemini GV - Resolver to Encoder Signal Conversion
      • Gemini GV6 & GT6 RS232 Daisy-Chaining ERRLVL
      • Gemini Maximum Frequency Input and Output
      • Gemini OS Download Failures
      • Gemini Step & Direction Inputs
      • Gemini Update Rates.
      • Gemini Variable Resolution
      • Gemini: 400LXR Tuning
      • Gemini: ASCII or Binary?
      • Gemini: VIDEO: express basics training: How to Connect Ethernet (includes Win7)
      • Getting the letter a with a ~ over it in Motion Planner Terminal
      • GFB-KIT Pinout
      • GV Cable Diameters.
      • GV6K & GT6K cannot Follow Analog Onboard Input
      • GV6K Tuning in Position Mode with Motion Planner
      • Hall State Checking on Gemini Products
      • Hall-less Startup on Gemini
      • I cannot communicate with my GEM-6K.
      • Limits on Gemini
      • MS cable option vs. GS cable option
      • OS 1.70 Additions
      • Replacing the Gemini GC-SDA
      • RESET command in STARTP program
      • Resolution of the Gemini command signal.
      • RS232 Troubleshooting for the Geminis
      • Step & Direction Output
      • TASX Bit 1 -- Motor Temperature Fault
      • TASX Bit 10 - Bridge Fault (Hardware)
      • TASX Bit 11 -- Bridge Over-Temp Fault (Software)
      • TASX Bit 12 -- Over-Voltage Fault
      • TASX Bit 17 -- Stall Detected
      • TASX Bit 18 -- Override mode
      • TASX Bit 19 -- Foldback Active
      • TASX Bit 2 -- Low Voltage Fault
      • TASX Bit 20 -- Power Dissipation Circuit Active
      • TASX Bit 21 -- Bad Hall State Detected
      • TASX Bit 22 -- Unrecognized Hardware Detected
      • TASX Bit 23 -- User Fault Input Active
      • TASX Bit 24 -- Keep Alive Circuit Active
      • TASX Bit 25 -- Power Dissipation Circuit Fault
      • TASX Bit 28 -- Motor Configuration Warning
      • TASX Bit 29 -- ORES Failure
      • TASX Bit 3 -- Drive Temperature Fault
      • TASX Bit 30 -- Motor Thermal Model
      • TASX Bit 31 -- Commanded Torque Limit Hit
      • TASX Bit 5 -- Encoder/Resolver Failed
      • TASX Bit 7 -- Motor Configuration Error
      • TASX Bit 8 -- Incoming Pulses
      • TASX Bit 9 -- Velocity Error Limit Exceeded
      • The GV and Linear Motors
      • Tuning a GV6K GV6 or GV in Position Mode
      • Tuning GV or GV6 drives with large inertia loads.
      • Tuning the Gemini in Position Mode
      • Tuning the Gemini in Position Mode.
      • Tuning the Gemini in Torque Mode.
      • Tuning the Gemini in Velocity Mode.
      • Using Gemini with Empire Magnetics Step Motors
      • VIDEO: Basics Training: GV or GT drives
      • VIDEO: Basics training: GV6 or GT6 drive controllers
      • VIDEO: Basics training: GV6K or GT6K drive controllers
      • What are Q and D currents?
      • What does the Error Log contain?
      • What drives can work with a DC brushed motor?
      • What happens in Keep Alive mode?
      • What motors with what Gemini drive?
      • What recognitions does the Gemini GV have?
      • What replaces the Gemini GT stepper drive?
      • What replaces the Gemini GT6 stepper drive/controller?
      • What replaces the Gemini GT6K stepper drive/controller?
      • What replaces the Gemini GV6K servo drive controller?
      • Which Motors Work with GV-L Drives? GV-U Drives?
      • Which rotation is considered positive for GV6K?
      • Why doesn't my Drive I/O cable tighten down securely when using the jackscrews?
      • Why will my PAD and PED not update on the Gemini?
      • Z channel output from the Gemini?
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
TASX Bit 10 - Bridge Fault (Hardware)

Print Friendly and PDF
This fault typically indicates a short circuit in the motor or motor power cable. If power can be cycled to the drive and the bit clears (following removal of the motor power cable from the drive), then odds are that the drive has not suffered permanent damage. However, this bit can also be triggered by a physical failure of the bridge rectifier within the drive. Bridge over-current or a voltage spike can cause damage of this severity. If the fault is caused by a physical failure, the bit will not clear under any circumstances, and will remain active after cycling drive power. In this case, the unit will need to be sent in for repair or component replacement.

REMEDIES:

If this bit is always active regardless of what you do, then the drive is most likely damaged and needs to be repaired.

If this bit only goes active when a DRIVE1 is issued, and can be cleared by either...
A) disabling and re-enabling the drive, or by
B) cycling power,
...check the motor's power wiring to
the drive. Then confirm that the proper motor configuration file has been downloaded into the drive.
If this bit only occasionally goes active, then there are two likely causes with a third cause that is rather unlikely:

1) An intermittent short in the motor or motor cable. The only way to find this is by swapping out one component at a time until you are confident that the failure has gone away.

2) Electrical noise causing voltage spikes at the sensor inside of the drive can cause the drive to register this fault. Compare the installation to the EMC Installation guidelines in the Hardware Installation Guide. Make sure that the motor cable's shielding is properly connected at both the drive and motor ends of the cable.

3) The Current Loop that controls the current going to the motor becomes unstable and spikes the drive with current. This can occur with motors that have really low inductance. Certain motor designs, like Parker's BE16, can also cause it because the inductance significantly drops during operating of the motor as it heats up. Sudden motor jams also can cause the current to spike. Reduce the current loop gain (DIBW) to reduce the responsiveness of the Current Loop.
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply