Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Vix- Option 1 (MPM) Encoder Hardware Setup
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Vix- Option 1 (MPM) Encoder Hardware Setup
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)-
      • Analog control of a Vix stepper
      • Can an Intelligent ViX-In be Programmed as a Drive
      • Configuring the ViX-drive
      • DC Brushed Motor with a ViX
      • Does the Vix have software limits?
      • Downloading Programs
      • Easi-V with Windows 7 or Windows 10
      • Homing move not complete
      • How Do I Check encoder position?
      • How to program an intelligent ViX Stepper as a Step & Direction
      • LOADENC and SCALE Commands
      • Running a Rotary Motor with a ViX-xH
      • Sample Program - Move Continuously, Stop on Inputs
      • VIX - RS232 connections
      • VIX Servo: How to Home to a Hard Stop
      • VIX Update Rates
      • ViX User Variables
      • ViX CANopen / RS-485 option
      • ViX Easi-V Error Message: Invalid data read for limits mode
      • ViX Encoder Resolution / Input Frequency
      • ViX Motor files for non-preferred BE windings
      • ViX Tuning
      • ViX servo drive Z channel encoder output
      • ViX-RJ45 RS-232 Daisy-Chain Cables
      • ViX: Connector Part Numbers
      • ViX: ViX Update Rates
      • Vix- Option 1 (MPM) Encoder Hardware Setup
      • Vix-IE with Brushed motor and Encoder
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
Vix- Option 1 (MPM) Encoder Hardware Setup

Print Friendly and PDF
This FAQ allows the user to setup Option 1 Encoder motors with software changes. Option 1 Encoder motors can also be setup through software changes. Please see "ViX - (MPM) Encoder Option 1 Software Setup."
The following is a table for the MaxPlus (MPM) Encoder Option 1 Termination to ViX Connections:
Feedback Connections
ViX Feedback Connector X2Option 1 Encoder Cable (175-0xxx)***
Wire FunctionPin#Pin LetterFunction
GND3TGND
+5 VDC output5K+5VDC
incremental enc.A+8CCH A\
incremental enc.A-7BCH A
incremental enc.B+12NCH B
incremental enc.B-11PCH B\
incremental enc.Z+1MCH Z
incremental enc.Z-2UCH Z\
Commutation f-b A09ECH U
None*N.C.*RCH U\
Commutation f-b A113FCH V
Commutation f-b A214GCH W
None*N.C.*SCH U\
None*N.C.*HCH W\
Connector Housing****DGnd/CableDrain
Motor overtemp+ 10ATHERM
Motor overtemp-6LTHERM
Connector Housing****JSHLD

Motor Power Connections
ViX Motor Power Screw TerminalsOption 1 Motor Power Cable
X1 FunctionPhasePin LetterFunctionWire Color
Phase UUAPhase RRed
Phase VVCPhase TBlue
Phase WWBPhase SBlack
GroundGNDDPE GND


*The Hall signals on the MPM motors are diffential, therefore, you do not need to connect the negative signals of each hall state to the single-ended ViX Hall signals.
**The shield connections of the feedback cable should be connected to the ViX X2 header's metal housing (if possible).
*** Option 1 encoder cable wire colors can vary, however, the wire function should be consistent among all cables. If your cable wire marker (labels) are no longer present or readable, please contact Parker.
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply