Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller-
      • IPA Accessories - IPA as Ethernet/IP Scanner for Ethernet/IP I/O Adapter Devices (Video)
      • IPA Cables - P Series Motors to IPA
      • IPA Hardware - Connector Part Numbers
      • IPA Hardware - DC Power
      • IPA Hardware - Does the IPA Have Battery Backed Memory or Flash?
      • IPA Hardware - MX80L Limit/Home Wiring
      • IPA Hardware - Short Circuit Current Rating (SCCR)
      • IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)
      • IPA Hardware - What is the minimum regen (braking) resistor value allowed?
      • IPA Misc - Letter of Volatility
      • IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)
      • IPA Misc - Absolute Encoder Compatibility (EnDat)
      • IPA Misc - Aries Controller Replacement
      • IPA Misc - How to Calculate Regeneration
      • IPA Misc - How to Change the IP Address
      • IPA Misc - IPA with Allen-Bradley Ethernet/IP with ETH Actuator (Video)
      • IPA Software - Add On Instructions Tutorial for Allen-Bradley Logix PLCs (Training Video)
      • IPA Software - Add-On Instructions
      • IPA Software - Analog Input Parameters, Filtering, Example Joystick Program (Video)
      • IPA Software - Assigning Limit and Home Inputs (HLBIT)
      • IPA Software - Basic Tuning using ACR-View
      • IPA Software - Change Direction of Travel (What is Positive/Negative Motion)
      • IPA Software - Communicating via ASCII over Ethernet TCP/IP
      • IPA Software - Configuration Parameter for the Feedback Type
      • IPA Software - Ethernet/IP with Allen-Bradley or Omron PLCs
      • IPA Software - Example - Ballscrew Compensation / Slope Correction
      • IPA Software - Example - Cable Winding Application
      • IPA Software - Example - Error Recovery Program
      • IPA Software - Example - Excel Spreadsheet to Upload/Download Arrays
      • IPA Software - Example - How to Home to a Hardstop
      • IPA Software - Example - Interact Xpress HMI
      • IPA Software - Example - Torque Limited Move for Clamping (with Video)
      • IPA Software - How does motion work in the ACR products (ARC7xxx, ACR9xxx, IPA, Aries-CE)
      • IPA Software - How to Change the Home Start Direction and Other Home Settings
      • IPA Software - How to Save Servo Gains
      • IPA Software - INTCAP (Position Capture)
      • IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range
      • IPA Software - Torque Enable Inputs Functionality
      • IPA Software - User Variables and Bits (Which are retained?)
      • IPA Troubleshooting - Endat Absolute Encoders with IPA-Feedback Errors
      • IPA Troubleshooting - ETT Actuator Noise
      • IPA Troubleshooting - PC communications (Ethernet)
      • IPA Troubleshooting - Watchdog Timeout Event Triggered or Reconnect Event Triggered Error (ACR-View)
      • IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?

Print Friendly and PDF

Applies to IPA, all ACR7xxxx and ACR9xxx products, and the discontinued Aries-CE.

There are several reasons your HMI or GUI may not be able to access the ACR language user parameters P0 - P4095.

First, user parameters P0 - P4095 do not exist by default in any of the ACR language products.  These user parameters must be dimensioned in memory at the time your main configuration is done, typically via the ACR-View configuration wizard.  If these are not dimensioned in memory then they do not exist in that particular project and cannot be accessed in that particular controller. 

Second, these are 64 bit floating point user parameters.  Many HMI drivers (like Interact Xpress and InteractX) only support 32 bit data types so you may be able to access smaller values and then get bad responses if the values are larger.  We recommend using P39168 - P39423 which are 32 bit float data type or P38912-P39167 which are long data type and have the added advantage of being non-volatile in most of the ACR controllers.

Finally, your HMI driver or GUI may be doing direct memory access via the binary host protocol that the ACR language supports (PEEK and POKE functions).  The recommended procedure for this is out-lined in the ACR Programmer's Guide in the Binary Host Interface chapter.     ACR Programmer Guide

The address for a particular parameter should be requested before attempting to PEEK or POKE information.  If the address is returned as zero then the particular parameter or local array is not dimensioned.  Also, the actual address locations of specific parameter groups (such as the user parameters P0 - P4095) may vary from product to product or revision to revision so hard coding these addresses can lead to problems.

For example, the P0 - P4095 parameters reside in different memory locations between the ACR9xx0 controllers, Aries-CE drive/controllers, and IPA drive/controllers. 

Interact Xpress HMI Interact X HMI Red Lion HMI

IPA04-HC IPA15-HC AR-04CE AR-08CE AR-13CE  ACR9000 ACR9030 ACR9040 ACR9600 ACR9630 ACR9640

glh 4/2017

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply