Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base VS Motors - Wiring and Currents
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base VS Motors - Wiring and Currents
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
  • AC/DC Industrial Drives+
  • Servo Motors+
  • Step Motors-
    • A/AX Motors - A vs M motors
    • eCLM Motors - Stepper motor Resonant speeds
    • General - Checking Stepper Motor Phases.
    • General - Connectors on Step Motor Cables?
    • General - Custom Stepper Motors
    • General - Encoder Option Clarification for Step Motors (-EC or -E options )
    • General - How many steps per revolution do our motors have?
    • General - Operating Temperature Range for Stepper Motors
    • General - Series vs Parallel wiring in motors
    • General - Step Drive and Motor Compatibility Chart (older legacy lines)
    • General - Stepper Cross-Over Chart (discontinued models)
    • General - Stepper Motor Fault.
    • General - Steppers: Determining Pinouts
    • General - Unipolar and Bipolar motors.
    • General - Unipolar Drive Wiring with Bipolar Motors
    • General - Why is my stepper motor getting hot?
    • LV/HV Motors - Customs
    • LV/HV Motors - HV and LV 34 Frame Stepper Motor Round Shaft Option
    • LV/HV Motors - IP rating on stepper motors?
    • LV/HV Motors - Purple or Red/White Wire
    • LV/HV Motors - Replacements for the VS series step motors
    • LV/HV Motors - Step Motor Wiring
    • LV/HV Motors - Stepper Motor Order Code
    • LV/HV Motors - Stepper motor Resonant speeds (Waveform, Balance, Offset)
    • OEM Motors - Connector Part Numbers
    • OEM Motors - OEM Step Motor Part Numbers
    • PK Motors - PK162-308 Specifications
    • Replacing S106 or TS41 TS42 TS43 step motors with Servo Motors
    • S/SX Motors - Motor inductance
    • S/SX Motors - Replacing S/ZETA/ES series step motors with BE servo motors
    • S/SX Motors - S106 Motor Replacements
    • S/SX Motors - S106 motor specifications
    • S/SX Motors - Step motors with Brad Harrison Connectors (Yellow 5 pin)
    • VS Motors - Motor Cables
    • VS Motors - Wiring and Currents
    • ZETA, S, ES Series Step Motors Discontinued & Suggested Replacements
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
VS Motors - Wiring and Currents

Print Friendly and PDF

Please read the FAQ titled Stepper Motor Current Settings, which contains very important details on how our motor currents are derived and what operating conditions must be met!

VS Motors with Zeta Series, OEMZL Series, S Series, E-AC, Gemini GT Series, or any 170 VDC bus voltage drive
Wiring diagrams and motor current values can be found in the E-AC Hardware Installation Guide and E-AC Quick Reference Guide. The motor current values in these guides apply to any Parker drive that utilizes a 170 VDC bus voltage.
NOTE: When configuring the Gemini GT Drive, the motor current values in the Gemini Setup Wizard of Motion Planner are correct and should always be used!!!

VS Motors with OEM750 Series, E-DC, or any 75 VDC or less bus voltage drive
Wiring diagrams and motor current values can be found in the E-DC Hardware Installation Guide and E-DC Quick Reference Guide. The motor current values in these guides apply to any Parker drive that utilizes a 75 VDC or less bus voltage.
NOTE: These current values are for parallel wiring only. In order to get a reasonable performance out of the motor, we require the parallel connection. However, with the parallel connection, we are only allowed the standard 50 % duty cycle (move time vs standstill time).
VS Motors with ViX Stepper Series, PD Series, or any Digiplan marked drive. The VS motor wiring and current settings for the ViX Stepper Series are located in the ViX Stepper User Guide. Please use the current settings that are set in the Guided Drive Setup Utility of the EASI-V software. The PD Series has a bus voltage of 70 VDC, so please refer to the E-DC guide as directed above for motor current values and consult the ViX Stepper User Guide for the wiring. For all other Digiplan products, please first consult the user manual to determine the bus voltage. If the bus voltage falls into the following two ranges (170 VDC or 24-75VDC) please use the motor current values from the appropriate section above. Again, please consult the ViX Stepper User Guide for proper wiring.
NOTE: The former Digiplan designed drives used a different motor phasing scheme than the Compumotor designed phasing scheme. Therefore, this was handled by swapping the wire colors for B+ and B- from the standard Compumotor phase/wire color scheme. Thus, this swap is documented in the ViX Stepper User Guide.


Parker Hannifin - Electromechanical Automation Division North America, http://www.parkermotion.com
All Product User Guides can be found at: Online User Guides

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply