Hi,
I'm controlling a AC10 over modbus RTU and everything is working fine. I have configured F905 to timeout if communication is lost, this is also working and the drive trip to CE.
However, the fault reset isn't working over modbus when the drive trip into Communication Timeout (CE). I can reset it localy on the drive and on the digital inputs. I have confirmed that in my program I'm sending 7 to command word wich is representing "fault reset", the modbus communication as stated before is also working fine running forward etc. How do I reset CE fault over modbus?
/Tim