Hello friends,
we have several C3 compax S075, exactly model C3 S075 V4 F10 I20 T40 M12. All running ok.
We have bought more devices, same model and we want copy the program from the drives that it's running to new devices for replacement if necessary.
I tried do it, using RS232 interface and C3 servomanager software but i couldn`t do it.
First i connect with one device and i make a UPLOAD of "device configuration" and created a file that i saved.
When i tried "DOWNLOAD" the file in the new device, it was impossible, several errors.
I have any questions:
1) Firmware and controller board it's different, i need it's the same?
2) Can i make this copy with RS232 interface?
3) To "clone" the device, only with "device configuration" it's enough or i need copy other parameters?
Thank you ver much!!!!