1- How to upload program from HMI XPR2 using IP Address and how to know IP Address of HMI?
2- How to upload program from HMI XPR2 using RS232 and how to do setting of this communication and the wiring of programming cables?
1- How to upload program from HMI XPR2 using IP Address and how to know IP Address of HMI?
2- How to upload program from HMI XPR2 using RS232 and how to do setting of this communication and the wiring of programming cables?
You will need to use Interact Xpress Manager for uploading and downloading.
Interact Xpress Manager is part number IXM-0310
Finding the IP Address of the unit involves going into the Xpress Shell->Setting->Network. If the unit boots up to the application, some programmers have programmed an Exit button that will Exit to the Shell.
If there is no Exit button, then you can remove the CF Card and then plug it into a CF Card Reader and PC. Interact Xpress Manager will then be able to upload the project from the CF Card.
More information on Interact Xpress Manager and the Shell can be found in Chapter 4 and 5 respectively in this document
http://divapps.parker.com/divapps/emn/download/Interact_Xpress/Ver_2.14/IXUG.pdf