Dear All ,
I get New Drive 590+ 70 A and I need to copy configuration from old drive 590+ 35 A
I have read to copy configuration by upload to OP then download but it for the same sating power
""How do I copy the configuration from one drive to another using the keypad?
1) Clone a drive configuration from one 590+ drive to another 590+drive.
NOTE: The drive firmware and the 6901 keypad (which must be FW 11v1 or newer) must both support cloning. If either firmware does not support cloning, the option to “SAVE TO OP” will not appear in the menu.
NOTE: A 690+ configuration from a firmware version 4.x drive can be installed into a version 5.x or 6.x drive.
NOTE: The drives you are cloning MUST be the same horse power/kW rating or the keypad will lose the configuration and the new drive will NOT be cloned.""
can I make it with any another way ???
using for example DSE lite Configuration Tool or can by using keypad