Print Friendly and PDF

DC Drive 590+ Frame 3

Hello!

DC Drive 590+ Frame 3 max.armature current 270A

I have the potentiometer  for the regulating speed!

Potentiometer connected to B3 +10V and A1 0V And to terminal A4 for the regulating!

Can i use the external +10 volts for the speed regulating?

I want take off the potentiometer and connect external +10 volts from the Scneider PLC Analog card!

I need regulate speed from the PLC

How can i make it better?

Best regards,

Dmitri