• Home
  • Investors
  • Contact Parker
  • Sign In / Register
Parker Community
  • Site
  • User
  • Site
  • Search
  • User
  • Products
  • Support
  • Divisions
  • Where to Buy
  • Careers
  • About Parker
Home Parker Community Technologies Electromechanical Group Electromechanical Knowledge Base Visual Basic Sample with AT Card
Sign In / Register

Sign In

Register
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
  • OEM Products+
  • C3 + Xpress + ETH+
  • Legacy-
    • 4000+
    • 6000-
      • 6000 Servo Products I/O Updates
      • 6000 Step Products Analog Inputs
      • 6250 Analog Input Option (-ANI)
      • 6250 and AT6250 Third Encoder Port
      • AT Servo Cards & Windows NT - OS Lock-Up
      • AT6000 Auxiliary Cables
      • AT6000 Product Issues
      • AT6200 and AT6400 are now CE marked
      • AT6XXX
      • AT6xxx Operating System Compatibility
      • AT6xxx Operating System Files
      • Auto-load operating system at startup
      • Backing up 6000 Programs
      • Bad DLL Calling Convention
      • Control Velocity with an Analog Input.
      • DDE 6000 and Excel
      • Downloading Programs in a Daisy Chain
      • Home Backup Controls Cluster with Motion Toolbox
      • Homing to Z channel on 6000 products
      • HOMLVL command
      • How do I change velocity on the fly during JOGGING?
      • How do I make a program run on power up?
      • How do I make a proper back up for my 6000 series controller?
      • How to send/receive with OCX
      • Input Buffer for 6000 Serial Producs
      • Input Debounce Times for 6000 Series Products
      • Input Impedance for -ANI option for AT6n50
      • Interrupts, AT cards & troubleshooting
      • Linker Error
      • LSCW and LSPOS are the same command
      • Minimum files for AT card
      • Model 6201 Information
      • Motion Architect and WinRT
      • Motion Toolbox in a Daisy Chain
      • PCOMP in Conditional Statements
      • Reading in multiple numbers with the TM8
      • ReceiveFile method bug
      • RecvAT6400Block documentation error
      • Running more than 199 programs in 6000 Products
      • Scaling With the 6000 Products
      • Sequence Names Can Cause Problems.
      • SetNTMultiCardAddress doc error
      • Status Bits and Commanding a Velocity of Zero
      • Unable to get Procaddress32W for wrtoutpw error
      • VIDEO: DDE Server - Communicating from MS-Excel
      • Visual Basic Sample with AT Card
      • What addresses are in use on my NT machine?
      • What can I use as a replacement for my 6200 or OEM6200 indexer?
      • What can I use as a replacement for my 6250 or OEM6250 servo controller?
      • What can I use as a replacement for my AT6200 or AT6400 indexer?
      • What can I use as a replacement for my AT6250 or AT6450 servo controller?
      • What is WinRT anyway?
      • Why does RESET6000.VI cause error 5004 in Labview?
      • Why is my AT-card locking up?
      • Why is the motor not moving when I command it to?
      • X language to 6000 series language
    • APEX & APEX615x+
    • BLOK+
    • Compucam+
    • Digiplan BD, BDS, BDHX,BL, BLX,BLHX, PDS, PDX, PDHX+
    • iBE+
    • L20+
    • MP-FLX+
    • MPA Servo Drives+
    • Motion Architect+
    • PC21+
    • RP240+
    • S/SX Drives+
    • SFD Servo Drives+
    • SLVD & HPD+
    • TBF & TBN Servo Drives+
    • TQ10 & TQ10X+
    • XWare / X Language+
    • Z ZX ZXF Drives+
    • Downloading from the FTP site
    • MTS Automation / Custom Servo Motor User Guides and Documentation Location
    • Retired Products
    • Torque, Velocity & Position Loops
  • Other+
  • Technologies
    • Aerospace
    • Climate Control
    • Electromechanical Group
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Blogs
  • Forums
  • Knowledge Base
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

Visual Basic Sample with AT Card

Print Friendly and PDF
Here is a sample flow diagram of how to can check if motion has stopped on a particular axis. The example is for an AT product under Visual Basic 4.0 environment.

Using the "Fast Status" capability of the AT6400 you may check a bit in a register. This bit will tell you if your motor is moving or not. A good idea would be to create a subroutine that waits for your motor to stop moving. Check Chapter 2 of the "6000 Series Programer's guide" for more details.

A sample is written below. The steps are as follows:

Step 1
Make a function that returns a TRUE if the motor is currently moving and a FALSE if the motor is not moving. Call the function IsMoving(....)

Arguments: Axis
This argument specifies which axis to check for motion.

Return Values: Boolean
TRUE if specified Axis is moving.
FALSE otherwise.

Step 2
Make a subroutine that waits for motion to stop. Call the subroutine WaitForMove(.....)

Arguments:Axis
Same as above.


Sample Program follows:

Public Function IsMoving(ByVal Axis As Integer) As Boolean

Dim status_high As Integer
Dim status_low As Integer
Dim status As Long

Dim Temp As Integer
Select Case Axis

Case 1
Temp = request_status(Address)
Call set_pointer(Address, AXIS1_STATUS)
Call read_status(Address, status_high, status_low, status)
IsMoving = status And 1 'Mask out all bit so that only bit one remains

Case 2
Call set_pointer(Address, AXIS2_STATUS)
Call read_status(Address, status_high, status_low, status)
IsMoving = status And 1 'Mask out all bit so that only bit one remains

Case 3
Call set_pointer(Address, AXIS3_STATUS)
Call read_status(Address, status_high, status_low, status)
IsMoving = status And 1 'Mask out all bit so that only bit one remains

Case 4
Call set_pointer(Address, AXIS4_STATUS)
Call read_status(Address, status_high, status_low, status)
IsMoving = status And 1 'Mask out all bit so that only bit one remains

Case Else
IsMoving = False

End Select

End Function

'This subroutine waits for axis to stop moving

Public Sub WaitForStop(ByVal Axis As Integer)

Do Until IsMoving(Axis) = False
Temp = DoEvents()
'have this loop wait

Loop
End Sub


Now if you start a motion on axis 1 just call the WaitForStop(1) funtion and it will wait until all motion has stopped.

Example:

Call MakeMove(1) 'make axis 1 move
Call WaitForStop(1) 'wait until axis one has stopped moving.
  • Share
  • History
  • More
  • Cancel
Related
  • Technologies
    • Aerospace
    • Climate Control
    • Electromechanical Group
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
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
Parker - Engineering Your Success
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
Ā© Parker Hannifin Corp 2019