Home Technologies Electromechanical Group Electromechanical Knowledge Base System Pointer Address of ACR Global Variables, P0-P4095
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base System Pointer Address of ACR Global Variables, P0-P4095
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
System Pointer Address of ACR Global Variables, P0-P4095

Print Friendly and PDF

Supplement to ACR Programmers Guide,Binary Host Interface "Application: Binary Global Parameter Access"

The memory address for the global user variables (P0-4095) can be read at the "System Pointer Address" Each controller has a different address based upon it's firmware:

AR-xxCE  0xA0600020
ACR9000 0x400009     (same for 9030,9040,9600,9630,9640)
ACR8020 0x400009
ACR8010 0x403E08
ACR8000 0x403E08
ACR2000 0x400008
ACR1505 0x400009
ACR1500 0xC08008
ACR1200 0x400008

This could be used with the ComACRserver's "GetACRMemory" to retrieve the value of up to 255 global variables at a time.

Using the GetACRMemory for the above address retrieves the Global_Variable_Address. 

If the returned address is zero, there are no dimensioned global variables (see the DIM command).

If the returned address is other than zero, use GetACRMemory at this address to receive the number of dimensioned global variables.

Read a global variable P(index) using the following addressing scheme for Peek: 

Peek address = Global_Variable_Address + 1 + ( index * 2 )
Where index = 0 to ( number of dimensioned global variables - 1 )

Even though global variables are stored on-board as floating point 64 (FP64) numbers, they are returned as IEEE32 numbers.
 
Note for Aries Controller (AR-xxCE), all memory accesses are byte addresses, so the equation to access globals on the CE is different:
Peek address = Global_variable_address + 4 + (index*8), where index = 0 to (number of globals-1).
 
Update 23-Mar-2012 JW
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.