Home Technologies Electromechanical Group Electromechanical Knowledge Base What is the Binary Host Interface
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base What is the Binary Host Interface
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
What is the Binary Host Interface

Print Friendly and PDF

Products: ACR9000, 9030,9040,9600,9630,9640, Aries Controller (AR-xxCE)

The ACR controller can be interfaced to a PC application through the provided COM object. The controller is delivered with a software development kit called ACR-View, which installs the COM object: ComACRserver. The ComACRserver provides methods and functions that allow the user to create custom PC applications in VB, C++, .NET,LabView, etc to command the controller via Ethernet, USB, or serial.  

The ComACRserver is a wrapper for the lower level communication called the Binary Host Interface. Most application will use the ComACRserver but some users prefer to use the native Binary commands directly. Using the Binary Host Interface natively allows users to optimize the performance of applications by eliminating the COMACRservers overhead. It also provides a communication option for non-Windows applications (e.g. Linux) as the ComACRserver uses the MS COMobject model.

Details about the Binary Host Interface can be found in the ACR Programmers Guide within ACR-Views on-line help, or download the PDF version here.

Serial:
When using the Binary Host Interface with serial communication, by sure to read and follow the user discussion about MODE and Control Character Prefixing in the section called Binary Data Transfer.
 
Ethernet:

Details about Ethernet communications to the ACR controller can be found in the Ethernet Spec which describes the base level TCP and UDP connections and data formats.

Port 5002 is an ASCII connection. With this connection you could send any Acrobasic command to the controller as if you were in the terminal emulator in ACR-View.

Port 5006 is a managed binary connection that expects to see commands in a specifc format. 5006 is well suited for PC applications and constructing drivers.
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.