Home Technologies Electromechanical Group Electromechanical Knowledge Base What replaces my old CTC powerstation that is running Interact?
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base What replaces my old CTC powerstation that is running Interact?
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver+
    • Interact (Legacy)+
    • InteractX+
    • Interact Xpress+
    • IX / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (DOS-based Interact HMI)-
      • PS Series PowerStation will not boot up,
      • Removing the splash screen from the P9 or PS?
      • Weight of my PS-Series PowerStation
      • What replaces my old CTC powerstation that is running Interact?
      • How to get the application off old HMIs running Interact
      • MotionPanel replacement
      • Obsolete P1x-xxx or PMP-xxx P12-xxx or P1P-xxx or P1H-xxx ending in AR or DR and the P15 P1-10" manuals.
      • UDP Network traffic when Interact HMI installed
      • Upgrading your Interact HMI - Boot Drive / Storage Warning for P11-xxxxR, P21-xxxxR Model Number format and Models starting with PWR
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
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
What replaces my old CTC powerstation that is running Interact?

Print Friendly and PDF
Old Unit Replaced By Software Required Notes
P11/PMP/P1H
6" QVGA
320x240
P1306QT-Q3 Interact 7 (Windows XP) For Class 1 Div 2, replace ending 3 with 5
P12-3##
6" QVGA
320x240
P1306QT-Q3 Interact 7 (Windows XP) For Class 1 Div 2, replace ending 3 with 5
P12-4##
6" VGA
640x480
P1306VT-Q3 Interact 7 (Windows XP) For Class 1 Div 2, replace ending 3 with 5

Information on the P13 Family can be found at the following link:

http://www.parkermotion.com/products/Dedicated_HMI__5937__30_32_80_567_29.html

Old Unit Replaced By Software Required Notes
P15/P2x/P3x/P4x/P5x/PS10/PA10 PA210T-133 Interact 7 (Windows XP) For Class 1 Div 2, replace ending 3 with 5
PA06S (PA05S - no 5" units) PA206Q-133 Interact 7 (Windows XP) For Class 1 Div 2, replace ending 3 with 5
PA08S PA208T-133 Interact 7 (Windows XP) For Class 1 Div 2, replace ending 3 with 5
PA15T/PS15 PA215T-133 Interact 7 (Windows XP) For Class 1 Div 2, replace ending 3 with 5

Information on the PA2 Family can be found at the following link:

http://www.parkermotion.com/products/Dedicated_HMI__7292__30_32_80_567_29.html

Keep in mind the following BEFORE ordering a new unit.

1. The PA2 and P13 series do not support PC104/ISA bus cards.  If you are using these, please re-evaluate the application.

2. The PA2 and P13 series ONLY has 2 serial ports.  If you are using more than 2 serial connections or printing from LPT1, please re-evaluate the application.

We no longer manufacture hardware with 3 com ports or Parallel Printer Ports that can run MSDOS Interact Runtime.

3. Interact Software upgrade is REQUIRED.  Interact Software is only compatible with Windows XP and will not work in Window 7 XP Mode. 

4. Interact software is an additional purchase.

Interact:

  • PA2 units are pre-loaded with (and require) Interact7 runtime.
  • ALL optional runtime modules are included with every PA2. With older versions of Powerstations like the PA, runtime modules were selected with additional cost to the hardware.
  • PA2s can run projects developed in older versions of Interact, but must first be upgraded using Interact 7
  • Interact 7 Development software Part numbers:
Model # Description
MSP-7NA0-P Interact7 Development (new user)
IUP-6070-6 Interact Development Upgrade to 7.X from 6.X
IUP-6070-5 Interact Development Upgrade to 7.X from 5.X

 

 Last Modified 3/27/2012 by KJAX

edited dom 07/24/2019

  • P7
  • P3
  • INTERACT
  • PS
  • PA
  • P1
  • HMI
  • P2
  • HPC
  • IPC
  • DOS
  • P4
  • PA2
  • P9
  • PowerStation
  • P5
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.