• Home
  • Investors
  • Contact Parker
  • Sign In / Register
Parker Community
  • Site
  • User
  • Site
  • Search
  • User
  • Products
  • Support
  • Divisions
  • Where to Buy
  • Careers
  • About Parker
Home Parker Community Technologies Electromechanical Group Electromechanical Knowledge Base Trilogy IForce Custom High Vacuum Options
Sign In / Register

Sign In

Register
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
  • Linear and Rotary Positioners-
    • IForce Linear Servo Motors & Positioners-
      • When should I used a linear motor stage?
      • What are the main precision application types for linear motor stages?
      • Can Parker provide custom linear motor stage solutions?
      • 110 WD0 Motor Specifications
      • 310 Coil Bar Side Mounting Locations
      • Air Cooling and Liquid Cooling Notes
      • Can I use the motor in vertical applications?
      • Current Derate for less <0.5pitch moves
      • D Dual parallel winding specs
      • Different types of linear motors
      • Do the magnets lose their magnetism with time?
      • Does the motor coil float between the magnets?
      • Hall-Effect, Home and Limit Module Wiring
      • High Pot Option
      • How do I select a linear motor?
      • How to Wire MHED Limit/Home/Halls Module
      • IForce Coil Compatibility in Vacuum Environments
      • Importance of mechanical alignment
      • Inspection Report
      • LEM Feedback Troubleshooting & Replacements
      • LME vs PLME Linear Magnetic Encoders
      • ML18 Track Weights
      • Motors used underwater or in the presence of oils
      • No motors listed in WinTips motor database?
      • Old IForce actuator part numbering
      • Omega 44004 Thermistor Info
      • Parker MotionSizer - Temperature Rise Calculation
      • Phasing Diagram
      • Renishaw Optical Encoders
      • Trilogy Electrical Pitches
      • Trilogy Extension Cables
      • Trilogy High Flex Cable Specifications
      • Trilogy IForce Cooling Options
      • Trilogy IForce Custom High Vacuum Options
      • Trilogy Motor Summary & Drive Compatibility
      • Trilogy Motors with Non-Parker Servo Drives
      • What amplifier do I use to drive the linear motor?
      • What are the minimum bend radii of Trilogy THF flex cables?
      • What voltage for IForce hall-effect sensors?
      • Which MHED is used within the positioners?
      • Why do some motors have steel laminations?
      • Why lamination designs skew or angle their magnets
      • Winding Tolerances and Resistance Measurement
    • MX80+
    • mSR+
    • Ripped Series Linear Motors & Positioners+
    • Manufacturer Grease Standardization
    • P8S Position Sensor order codes
    • What type of encoder options are available for the Trilogy Series?
    • What type of material is used for the base of the Trilogy Linear Motor Positioners?
    • LXR+
    • mPR+
    • XE+
    • XR+
    • ZP Wedge+
    • How can I know if a given actuator is suitable for use in a specific environment?
    • I need speed and accuracy over a long length. What type of actuator should I use?
  • Electric Cylinders+
  • T-Slot Aluminum Framing+
  • OEM Products+
  • C3 + Xpress + ETH+
  • Legacy+
  • Other+
  • Technologies
    • Aerospace
    • Climate Control
    • Electromechanical Group
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Blogs
  • Forums
  • Knowledge Base
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

Trilogy IForce Custom High Vacuum Options

Print Friendly and PDF
The Trilogy IForce linear servo motors are available in a vacuum compatible option (-V), orderable via the extranet E-Configurator.  The -V option allows guaranteed operation in high vacuum environments up to 10^-6 Torr, but we have customers successfully using the -V option motors in environments as high as 10^-7 Torr.  The -V option on motor coils adds air bleed holes to all blind mounting holes and includes a clean room processing.  In clean room processing components are devoid of human contact, machining oils and epoxy patching.  The -V option is also available on the IForce magnet tracks, which also adds air bleed holes to all blind mounting holes and clean room processing.
For those that need an extra degree of protection in even higher vacuums, Parker offers a couple of custom options available as outlined below.  These custom components must be ordered through our custom quote process on the Parker Extranet.
VAC 2 processing - This customization eliminates the painting and patching step in the manufacturing process of the linear motor coils.  Normally, voids in the epoxy encapsulation process are patched with filler, sanded smooth and then painted black.  These materials are susceptible to out-gassing at higher vacuum levels and can trap air behind them, thus the materials are eliminated in this step.  The result of VAC 2 processing is a swiss cheese effect in some areas of the coil encapsulation in which copper wires can appear to be exposed.  The copper windings, however, are fully insulated and pose no danger of arching or high pot problems.
PTFE Insulated Flying Leads - This customization replaces the standard Trilogy THF flex cables, and replaces with PTFE (Polytetrafluoroethylene or Teflon) insulated flying leads.  The PTFE insulation is much less susceptible to out-gassing than the PVC jacketing on the THF flex cables, and thus is more suitable to high vacuum environments.
  • Share
  • History
  • More
  • Cancel
Related
  • Technologies
    • Aerospace
    • Climate Control
    • Electromechanical Group
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
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
Parker - Engineering Your Success
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
Ā© Parker Hannifin Corp 2019