• Home
  • Investors
  • Contact Parker
  • Sign In / Register
Parker Community
  • Site
  • User
  • Site
  • Search
  • User
  • Products
  • Support
  • Divisions
  • Where to Buy
  • Careers
  • About Parker
Home Parker Community Technologies Electromechanical Group Electromechanical Knowledge Base What configurable I/O is available on the AC890?
Sign In / Register

Sign In

Register
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
  • AC and DC Drives and Inverters-
    • AC10+
    • AC30+
    • AC690+ Series+
    • AC890 Series-
      • What are the basic wiring connections for the AC890?
      • What software and communication cable are used for programming an AC890?
      • How to Install and Extract Parameters From a 890 or 890PX Drive Using DSE Lite?
      • 890 - Interact Xpress with the AC890
      • 890: Why am I getting over-voltage trips?
      • 890PX - Proper ethernet cable - Current Balance, Undervoltage, Missing Phase
      • Can I clone an 890 drive via the Keypad?
      • Can the AC890 be configured as an Active Front End (AFE)?
      • Can the AC890 be used in a load-sharing application?
      • Can the AC890 be used in an electronic lineshaft application?
      • Can the AC890 be used in an encoder following application?
      • Converting .001 file types to .prj file type
      • How can I get the DSE software?
      • How can I get the DSELite software?
      • How can I load different firmwares?
      • How can I recover from a COMMS CODE N error on the AC890
      • How can I troubleshoot Firewire problems?
      • How can the 890 family be configured?
      • How can the AC890 be reset to factory defaults?
      • How can you add an item to the OPERATOR MENU in an AC890?
      • How do I determine an 890 drive TAG NUMBER so it can be used in DSE890?
      • How do I know what firmware revision my AC890 is?
      • How do I make an 890 Phase move?
      • How do I startup & troubleshoot a PMAC motor on the 890?
      • Is the keypad detachable during operation?
      • Is there any additional information on troubleshooting 690+ and AC890 Frame K drives? (copy)
      • My 890 control board locked up when updating the firmware, how can I reset the control board?
      • The AC890 is enabled, and START is true, but the motor runs slow with high torque. Why?
      • The AC890's DC bus voltage is extremely high on power-up. Why?
      • The AC890PX DC bus voltage is extremely high on power up. Why?
      • What are the minimum and maximum 3-phase input voltage ratings on an 890SD, CD, CS and PX?
      • What are the reference power supplies available to terminal connections on the AC890?
      • What can I use to replace an 8902/RR/00/00?
      • What configurable I/O is available on the AC890?
      • What is the current overload rating for the AC890 drive?
      • What is the maximum operating altitude for the AC890?
      • What is the operating temperature for the AC890?
      • What kind of I/O is available on the AC890?
      • What options can be added to the AC890/890PX?
      • What safety standards does the 890 meet?
      • What slots I can put options in, and how do I install them?
      • What types of speed feedback are supported for the AC890?
      • Where do I find default configurations?
      • Why am I getting an Incompatible Power Board message?
      • Why can't I connect to my AC890 drive with the USB cable
      • Why is my AC motor running hot?
      • Why is the LED on the control board flashing 50% red and 50% green?
      • Why won't DIN3 stop my 890 drive with a default configuration in remote mode?
      • Why won't my AC890 inverter run my motor?
      • HOW DO I CONVERT AC890 UK/JDE PART NUMBERS TO US PART NUMBERS?
      • HOW DOES THE INVERSE TIME (OVERLOAD) FUNCTIONALITY PROTECT THE DRIVE (890)?
      • Runtime alert when connecting to or downloading a project to an 890 drive - DSEv3.10
    • DC590+ Series+
    • TS8000, DSI3, & DSI8000+
    • Legacy/Discontinued VFD Products+
    • What software and communication cable are used for programming?
    • DSE Lite and Drive Firmware Compatibility
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
  • Servo Motors+
  • Step Motors+
  • Linear and Rotary Positioners+
  • Electric Cylinders+
  • T-Slot Aluminum Framing+
  • OEM Products+
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
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
      • Mobile IoT
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Blogs
  • Forums
  • Knowledge Base
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

What configurable I/O is available on the AC890?

Print Friendly and PDF

For what type of I/O the 890 can come with see this FAQ.

Digital Outputs 1 & 2 can be configured to function as Digital Input 8 and Digital Input 9 respectively. By default DIN 8 /DOUT 1 and DIN 9 /DOUT 2 are configured as a Digital Outputs. They can be set up as Digital Input 8 and Digital Input 9 using the software DSE.

BROKEN IMAGE -- DCLIFFE

Procedure

  1. Using DSE, delete the connections going to DIG OUT 1, as shown. Also configure a Logic Reader as shown using Tag 482. Tag 482 is the hidden internal connection for Digital Input 8. Connect the Logic Reader output, to the block to turn off /on. In this case, it is connected to the Or gate. Digital Input 8 is located at terminal X15-08 on the 890 drive.
  2. To configure DIN 9 /DOUT 2 as a Digital Input follow the above instructions but set the Logic Reader for Tag 514. Digital Input 9 is located at terminal X15-09 on the 890 drive.
  3. These Digital Inputs 8 & 9, operate the same as Digital Inputs 1-7. If 24vdc is applied to the appropriate hardware terminals, the Digital Inputs go True. These inputs are independent of each other. One can be an input and the other can be an output.

  • [QuickLink for the 890 on Parker.com] - Manual, QuickStarts, Product Support, etc
  • [QuickLink for the 890PX on Parker.com] - Manual, QuickStarts, Product Support, etc

7NOV2016 LS

  • Output
  • IO
  • AC30
  • configurable
  • inputs
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
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
      • Mobile IoT
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
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
Parker - Engineering Your Success
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
Ā© Parker Hannifin Corp 2021