• Home
  • Investors
  • Contact Parker
  • Sign In / Register
Parker Community
  • Site
  • User
  • Site
  • Search
  • User
  • Products
  • Support
  • Divisions
  • Where to Buy
  • Careers
  • About Parker
Home Parker Community Technologies Electromechanical Group Electromechanical Knowledge Base How do I make an 890 Phase move?
Sign In / Register

Sign In

Register
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
  • AC and DC Drives and Inverters-
    • AC10+
    • AC30+
    • AC690+ Series+
    • AC890 Series-
      • What are the basic wiring connections for the AC890?
      • What software and communication cable are used for programming an AC890?
      • How to Install and Extract Parameters From a 890 or 890PX Drive Using DSE Lite?
      • 890: Interact Xpress with Parker-SSD AC890 Drive Products
      • 890: Why am I getting over-voltage trips?
      • Can I clone an 890 drive via the Keypad?
      • Can the AC890 be configured as an Active Front End (AFE)?
      • Can the AC890 be used in a load-sharing application?
      • Can the AC890 be used in an electronic lineshaft application?
      • Can the AC890 be used in an encoder following application?
      • Converting .001 file types to .prj file type
      • How can I get the DSE software?
      • How can I get the DSELite software?
      • How can I load different firmwares?
      • How can I recover from a COMMS CODE N error on the AC890
      • How can I troubleshoot Firewire problems?
      • How can the 890 family be configured?
      • How can the AC890 be reset to factory defaults?
      • How can you add an item to the OPERATOR MENU in an AC890?
      • How do I determine an 890 drive TAG NUMBER so it can be used in DSE890?
      • How do I know what firmware revision my AC890 is?
      • How do I make an 890 Phase move?
      • How do I startup & troubleshoot a PMAC motor on the 890?
      • Is the keypad detachable during operation?
      • Is there any additional information on troubleshooting 690+ and AC890 Frame K drives? (copy)
      • My 890 control board locked up when updating the firmware, how can I reset the control board?
      • The AC890 is enabled, and START is true, but the motor runs slow with high torque. Why?
      • The AC890's DC bus voltage is extremely high on power-up. Why?
      • The AC890PX DC bus voltage is extremely high on power up. Why?
      • What are the minimum and maximum 3-phase input voltage ratings?
      • What are the reference power supplies available to terminal connections on the AC890?
      • What can I use to replace an 8902/RR/00/00?
      • What configurable I/O is available on the AC890?
      • What is the current overload rating for the AC890 drive?
      • What is the maximum operating altitude for the AC890?
      • What is the operating temperature for the AC890?
      • What kind of I/O is available on the AC890?
      • What options can be added to the AC890/890PX?
      • What safety standards does the 890 meet?
      • What slots I can put options in, and how do I install them?
      • What types of speed feedback are supported for the AC890?
      • Where do I find default configurations?
      • Why am I getting an Incompatible Power Board message?
      • Why can't I connect to my AC890 drive with the USB cable
      • Why is my AC motor running hot?
      • Why is the LED on the control board flashing 50% red and 50% green?
      • Why won't DIN3 stop my 890 drive with a default configuration in remote mode?
      • Why won't my AC890 inverter run my motor?
    • DC590+ Series+
    • TS8000, DSI3, & DSI8000+
    • Legacy/Discontinued VFD Products+
    • What software and communication cable are used for programming?
    • DSE Lite and Drive Firmware Compatibility
    • How to Update Drive Software
    • Software Matrix
    • How can I flash the LinkNet Techbox firmware?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
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
  • OEM Products+
  • C3 + Xpress + ETH+
  • Legacy+
  • Other+
  • Technologies
    • Aerospace
    • Climate Control
    • Electromechanical Group
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Blogs
  • Forums
  • Knowledge Base
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

How do I make an 890 Phase move?

Print Friendly and PDF

AC890 Phase Control

The 890 drive supports the Phase Move which is a simple trapezoidal relative move, to the master (it is added to the speed demand). It acts on each rising edge of the Enable input. The slave shaft is moved a fixed distance at a rate given by the Velocity parameter. A move must be completed before a new move will be registered. See Figure 3 for a Functional Description.

Equipment

890 Drive operating in the Closed Loop Vector mode and the software DSE890 or DSELite. An Encoder or Resolver must be mounted to the motor, and the 890 drive must be equipped with the proper Feedback option card. A FireWire option card is not required on the drive.

Description of the 890 System Blocks

BROKEN IMAGE -- DCLIFFE
Figure 1: Phase Move block.

Enable: Starts the Phase Move operation when going from False to True. Setting the Enable to False while a move is Active, will not abort the operation. This parameter is interlocked with the Position Loop block, thus Position Loop / Enable must be True before the Phase Move / Enable goes True. To abort the Phase Move once the operation starts, set Phase Move / Reset to True. When this is done, all Phase Move data will be lost.

Distance*: Sets the coarse distance (in motor revolutions) that the move command, will add to the phase loop. The range of this parameter is 3000.00000 to - 3000.00000 (motor revolutions). A negative (-) distance indicates that the motor will rotate reverse.

Distance Fine*: Additional Distance to allow fine control of position. The range is 3000.00000 to -3000.00000.

Velocity %*: The maximum velocity at which the distance is added to the phase loop. Velocity is a % of the Max Speed parameter. Thus if Max Speed = 1800 RPM and Velocity = 90%, the actual Velocity = 1800 x 0.9 =1620 rpm. The range is 0.100000 to 300.00000%.

Acceleration %*: The acceleration at which the distance is added to the phase loop. The acceleration, at which the distance is added to the phase loop, set in units per second squared.

Distance Left: Diagnostic showing the distance remaining before the move is complete.

Active: Will be True when the Distance Left is not zero.
*NOTE: If these parameters are changed during a Phase Move, the new data will be ignored until the move is completed.

Function Block Setup

The following parameters must be changed from the default to perform a Phase Move when using a stand alone drive:

  1. In the In the COMMS CONTROL block set FIREWIRE REF SEL to True.
  2. In the VIRTUAL MASTER block set CHANNEL to 1.
  3. In the FIREWIRE REF block set CHANNEL to 1.
  4. In the POSITION LOOP block set ENABLE to True.
  5. To make a phase move, PHASE MOVE / ENABLE must receive a logic True signal.

Setup Procedure

  1. Make sure that the drive has been Auto tuned and the drive is operating in the Closed Loop Vector mode.
  2. Set the desired Distance, Velocity & Acceleration values, in the Phase Move block.
    1. Example: If the Distance is set to 1.0, the motor will rotate 1 revolution when the Phase Move / Enable is set True.
    2. Example: If the Distance is set to 100.0, the motor will rotate 100.0 revolutions when the Phase Move / Enable is set True.
    3. Example: If the Distance is set to -100.0, the motor will rotate -100.0 revolutions (reverse motor rotation) when the Phase Move / Enable is set True.
  3. Start the 890 drive. (Enable Run Forward). When Phase Move / Enable goes True, the Phase Move / Active becomes True, the motor will rotate at the values set in the Phase Move block. The Phase Move / Distance Left will count backward toward 0. When the operation is completed, the Phase Move / Active becomes False and the value added to the Speed Loop from these blocks will be 0.
BROKEN IMAGE -- DCLIFFE
Figure 2


BROKEN IMAGE -- DCLIFFE
Figure 3: Functional description of a phase move.
  • [QuickLink for the 890 on Parker.com] - Manual, QuickStarts, Product Support, etc
  • [QuickLink for the 890PX on Parker.com] - Manual, QuickStarts, Product Support, etc

8NOV2016 LS

  • move
  • phase
  • control
  • 890
  • Share
  • History
  • More
  • Cancel
Related
  • Technologies
    • Aerospace
    • Climate Control
    • Electromechanical Group
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
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
Parker - Engineering Your Success
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
Ā© Parker Hannifin Corp 2019