• Home
  • Investors
  • Contact Parker
  • Sign In / Register
Parker Community
  • Site
  • User
  • Site
  • Search
  • User
  • Products
  • Support
  • Divisions
  • Where to Buy
  • Careers
  • About Parker
Home Parker Community Technologies Electromechanical Group Electromechanical Knowledge Base IPA Misc - How to Change the IP Address
Sign In / Register

Sign In

Register

  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller-
      • IPA Accessories - IPA as Ethernet/IP Scanner for Ethernet/IP I/O Adapter Devices (Video)
      • IPA Cables - P Series Motors to IPA
      • IPA Hardware - Connector Part Numbers
      • IPA Hardware - DC Power
      • IPA Hardware - Does the IPA Have Battery Backed Memory or Flash?
      • IPA Hardware - MX80L Limit/Home Wiring
      • IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)
      • IPA Hardware - What is the minimum regen (braking) resistor value allowed?
      • IPA Misc - Letter of Volatility
      • IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)
      • IPA Misc - Absolute Encoder Compatibility (EnDat)
      • IPA Misc - Aries Controller Replacement
      • IPA Misc - How to Calculate Regeneration
      • IPA Misc - How to Change the IP Address
      • IPA Misc - IPA with Allen-Bradley Ethernet/IP with ETH Actuator (Video)
      • IPA Software - Add On Instructions Tutorial for Allen-Bradley Logix PLCs (Training Video)
      • IPA Software - Add-On Instructions
      • IPA Software - Analog Input Parameters, Filtering, Example Joystick Program (Video)
      • IPA Software - Assigning Limit and Home Inputs (HLBIT)
      • IPA Software - Basic Tuning using ACR-View
      • IPA Software - Change Direction of Travel (What is Positive/Negative Motion)
      • IPA Software - Communicating via ASCII over Ethernet TCP/IP
      • IPA Software - Configuration Parameter for the Feedback Type
      • IPA Software - Ethernet/IP with Allen-Bradley or Omron PLCs
      • IPA Software - Example - Ballscrew Compensation / Slope Correction
      • IPA Software - Example - Cable Winding Application
      • IPA Software - Example - Error Recovery Program
      • IPA Software - Example - Excel Spreadsheet to Upload/Download Arrays
      • IPA Software - Example - How to Home to a Hardstop
      • IPA Software - Example - Interact Xpress HMI
      • IPA Software - Example - Torque Limited Move for Clamping (with Video)
      • IPA Software - How does motion work in the ACR products (ARC7xxx, ACR9xxx, IPA, Aries-CE)
      • IPA Software - How to Change the Home Start Direction and Other Home Settings
      • IPA Software - How to Save Servo Gains
      • IPA Software - INTCAP (Position Capture)
      • IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range
      • IPA Software - Torque Enable Inputs Functionality
      • IPA Software - User Variables and Bits (Which are retained?)
      • IPA Troubleshooting - Endat Absolute Encoders with IPA-Feedback Errors
      • IPA Troubleshooting - ETT Actuator Noise
      • IPA Troubleshooting - PC communications (Ethernet)
      • IPA Troubleshooting - Watchdog Timeout Event Triggered or Reconnect Event Triggered Error (ACR-View)
      • IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?
      • z CIP Communications stop on all devices when one CIP device goes offline (copy)
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
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
  • OEM Products+
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
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
      • Mobile IoT
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Blogs
  • Forums
  • Knowledge Base
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

IPA Misc - How to Change the IP Address

Print Friendly and PDF
The IP address for IPA Controllers can be assigned via hardware, programmed by the user or assigned dynamically from a DHCP server.
IPA Controllers ship with IP address default of 192.168.100.1
 
Switch Setting
Unit IP Address
Hardware
1 (S1=1, S10=0)
192.168.100.1
Hardware
2-98 (S1=2, S10=0)
Example: 14 (S1=4, S10=1)
192.168.100.(S10)(S1)
Software
99 (S1=9, S10=9)
User defined via IP command
Software
99 (S1=9, S10=9)
User defined via IP command
Set IP "0.0.0.0" or Set IP "255.255.255.255" to have the controller accept address from a DHCP server
Utility
0 (S1=0, S10=0)
192.168.100.1 (see note below)

Hardware Assignment:
 Change the switches to desired address in the range shown above then cycle power or issue REBOOT command for the new address to take effect.
 
Software Assignment:
Establish communication to the controller using a hardware assigned address. Change the hardware setting to 99 (S1=9, S10=9) but do not cycle power yet. In the terminal emulator assign a new address using the syntax IP "xxx.xxx.xxx.xxx".  Setting is saved automatically in non-volatile RAM.  Change subnet mask as needed using syntax IP MASK "xxx.xxx.xxx.xxx".  Cycle power or issue REBOOT command for the new address to take effect. For example:
SYS> IP "192.168.20.45"
SYS> IP MASK "255.255.255.0"
SYS>REBOOT

 

Utility:

There may be cases where a user program was created that is preventing communications. For example, a start-up program (PBOOT) includes the REBOOT command, which could cause the controller to repeatedly reset itself before communications can be established to kill and edit the program. The utility setting in the drive can be used to erase the programs and allow communications. 
Set the rotary switches to  0 and 0 and cycle power. The IP address will actually be 192.168.100.1, but the controller will not fully load the operating system. Use a terminal application such as Hyperterminal and connect to to 192.168.100.1, port 5002.  When connected the terminal will display the following:
Parker Hannifin Corporation
OS Loader Rev: 00.13
Remaining in OS Loader because:
IP address selected to 192.168.100.0
OSL>

At the prompt, enter  clear -user to erase user programs. 

OSL> clear -user
OSL>
Clearing user memory......DONE
OSL>

Change the IP address to a valid 1-99 value, cycle power and connect using ACR-View. 
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
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
      • Mobile IoT
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
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
Parker - Engineering Your Success
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
Ā© Parker Hannifin Corp 2021