Encoder mounted on the back:
- Plug in type encoder cable, NEMA 23 & 34
Extended motor cable - up to 200'
- integral to motor as opposed to spliced
Round shaft
Keyed shaft
Vacuum Rated
For brakes, we recommend using an in-line brake. Electroid has a brake line that does not require any additional holes as it mounts to the front face of the motor (FEB series) and has its own shaft out the front that mounts to the load.