• Home
  • Investors
  • Contact Parker
  • Sign In / Register
Parker Community
  • Site
  • User
  • Site
  • Search
  • User
  • Products
  • Support
  • Divisions
  • Where to Buy
  • Careers
  • About Parker
Home Parker Community Technologies Electromechanical Group Electromechanical Knowledge Base How can I make sure my DC motor does not have a problem with the Field Windings?
Sign In / Register

Sign In

Register
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
  • AC and DC Drives and Inverters-
    • AC10+
    • AC30+
    • AC690+ Series+
    • AC890 Series+
    • DC590+ Series-
      • How do I start troubleshooting a 590+?
      • What are the basic wiring connections required to run a motor, using the factory default drive?
      • How to Extract and Install Parameters to the 590+ Drive using DSE Lite
      • Why won't my motor run?
      • How can I make sure my DC motor does not have a problem with the Field Windings?
      • Why is my DC motor running hot?
      • 590+: Is the keypad detachable during operation?
      • Can I disable the field to run Brushed PMDC (Permanent Magnet DC motor) on a 590+?
      • Can I select between Manual Speed Reference and Line Speed Trim Setting for the same Analog Input?
      • Can you download a DSELite file into the drive when the drive is running?
      • How can I get the DSELite software the 590+ uses?
      • How can I make sure the motor will not start rotating until the speed pot is at 0?
      • How can I manually tune a 590+ drive to my motor?
      • How can I pre-trip "speed feedback" alarm before the drive trips?
      • How can I replace the control boards in 590+ Frame 1 and Frame 2 drives?
      • How can I set up a 590+ to be a field controller?
      • How can I upgrade a 590+ Frame 1 or 2 drive version 5.x or 7.x to version 8.x - Control Board and Configuration
      • How can the 590+ be programmed?
      • How can the drive configuration be reset to factory defaults?
      • How do I clone my 590+ Drive with the keypad?
      • How do I copy the configuration of one drive to another using the keypad?
      • How do I flash my 590+ drive to a newer Minor Revision of Firmware?
      • How do I know what firmware revision my 590+ is?
      • How do I set up a 590+ External Stack?
      • How to I configure the 590+ for Preset Speeds?
      • Is there anything I can check for a PRE SEQ READY alarm?
      • Modbus TCP/IP Addressing for the 590+ drive with the Ethernet Techbox
      • My DC590+ drive is displaying a Missing Pulse Alarm, what should I do?
      • The 590+ is enabled, but the main contactor doesn't close. Why?
      • Upgrading a control door from a 590 to a 590+
      • What accessories can be added to the 590+?
      • What analog and digital I/O is available on the 590+?
      • What are the Communication options for the 590+?
      • What are the communication settings for the 590+ for the P3 Port?
      • What are the differences between the 590 and 590+?
      • What are the minimum and maximum 3phase input ratings for the 590+?
      • What are the reference power supplies available to terminal connections on the 590+?
      • What are the types of Speed Feedback for the 590+?
      • What is the current overload rating for the 590+ drive?
      • What is the maximum operating altitude for the 590+?
      • What is the operating temperature for the 590+?
      • What safety standards does the 590+ meet?
      • What USB-serial adapter should I use?
      • Why does the drive fault to "Over-Voltage" after the drive is enabled?
      • Why does the drive fault to "speed feedback"?
      • Why does the drive fault to 3 phase-fail after the drive is enabled?
      • What I can I check for a CALIBRATION FAIL trip?
    • TS8000, DSI3, & DSI8000+
    • Legacy/Discontinued VFD Products+
    • What software and communication cable are used for programming?
    • DSE Lite and Drive Firmware Compatibility
    • How to Update Drive Software
    • Software Matrix
    • How can I flash the LinkNet Techbox firmware?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
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
  • OEM Products+
  • C3 + Xpress + ETH+
  • Legacy+
  • Other+
  • Technologies
    • Aerospace
    • Climate Control
    • Electromechanical Group
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Blogs
  • Forums
  • Knowledge Base
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

How can I make sure my DC motor does not have a problem with the Field Windings?

Print Friendly and PDF

Parker does not support rewinding motors in the field on our products, and do not recommend sending 3rd party motors to repair houses to be rewound. 

Improperly wound motors at repair houses are a common occurrence. "Improperly Wound" is defined as a motor not  being rewound to it's exact specifications on the nameplate. If exact values of inductance, resistance, field current, or voltage ratings are incorrectly implemented into the drive then instability in the control loop can occur. If implemented motor data is incorrect from the actual motor values due to being rewound (by an undefinable margin) then at best that instability causes a decrease in performance and control ability that may not be rectifiable. Worse, entire loss of functionality can occur due to the instability. 

We provide this below document as a means of verification of potential motor breakdown or if there are concerns that the motor is not up to specifications.

  • Link to document
[QuickLink for more Documentation for the 590+ on Parker.com] - Manual, QuickStarts, etc
13JUN19 JD - Update
  • motor
  • rewound
  • DC
  • Share
  • History
  • More
  • Cancel
Related
  • Technologies
    • Aerospace
    • Climate Control
    • Electromechanical Group
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
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
Parker - Engineering Your Success
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
Ā© Parker Hannifin Corp 2019