• Home
  • Investors
  • Contact Parker
  • Sign In / Register
Parker Community
  • Site
  • User
  • Site
  • Search
  • User
  • Products
  • Support
  • Divisions
  • Where to Buy
  • Careers
  • About Parker
Home Parker Community Technologies Electromechanical Group Electromechanical Knowledge Base How can I make sure my DC motor does not have a problem with the Field Windings?
  • Electromechanical Knowledge Base & Frequently Asked Questions
  • +Motion and Machine Controllers
  • +General Technology Information
  • +Virtual Engineer
  • +Visualization and Human Machine Interface (HMI)
  • +Servo Drives and Servo Drive/Controllers
  • +Stepper Drives and Stepper Drive/Controller
  • +Gearheads
  • -AC and DC Drives and Inverters
    • +AC10
    • +AC30
    • +AC690+ Series
    • +AC890 Series
    • -DC590+ Series
      • How do I start troubleshooting a 590+?
      • What are the basic wiring connections required to run a motor, using the factory default drive?
      • How to Extract and Install Parameters to the 590+ Drive using DSE Lite
      • Why won't my motor run?
      • How can I make sure my DC motor does not have a problem with the Field Windings?
      • Why is my DC motor running hot?
      • 590+: Is the keypad detachable during operation?
      • Can I disable the field to run Brushed PMDC (Permanent Magnet DC motor) on a 590+?
      • Can I select between Manual Speed Reference and Line Speed Trim Setting for the same Analog Input?
      • Can you download a DSELite file into the drive when the drive is running?
      • How can I get the DSELite software the 590+ uses?
      • How can I make sure the motor will not start rotating until the speed pot is at 0?
      • How can I manually tune a 590+ drive to my motor?
      • How can I pre-trip "speed feedback" alarm before the drive trips?
      • How can I replace the control boards in 590+ Frame 1 and Frame 2 drives?
      • How can I set up a 590+ to be a field controller?
      • How can I upgrade a 590+ Frame 1 or 2 drive version 5.x or 7.x to version 8.x - Control Board and Configuration
      • How can the 590+ be programmed?
      • How can the drive configuration be reset to factory defaults?
      • How do I clone my 590+ Drive with the keypad?
      • How do I copy the configuration of one drive to another using the keypad?
      • How do I flash my 590+ drive to a newer Minor Revision of Firmware?
      • How do I know what firmware revision my 590+ is?
      • How do I set up a 590+ External Stack?
      • How to I configure the 590+ for Preset Speeds?
      • Is there anything I can check for a SEQ PRE READY alarm?
      • Modbus TCP/IP Addressing for the 590+ drive with the Ethernet Techbox
      • My DC590+ drive is displaying a Missing Pulse Alarm, what should I do?
      • The 590+ is enabled, but the main contactor doesn't close. Why?
      • Upgrading a control door from a 590 to a 590+
      • What accessories can be added to the 590+?
      • What analog and digital I/O is available on the 590+?
      • What are the Communication options for the 590+?
      • What are the communication settings for the 590+ for the P3 Port?
      • What are the differences between the 590 and 590+?
      • What are the minimum and maximum 3phase input ratings for the 590+?
      • What are the reference power supplies available to terminal connections on the 590+?
      • What are the types of Speed Feedback for the 590+?
      • What is the current overload rating for the 590+ drive?
      • What is the maximum operating altitude for the 590+?
      • What is the operating temperature for the 590+?
      • What safety standards does the 590+ meet?
      • What USB-serial adapter should I use?
      • Why does the drive fault to "Over-Voltage" after the drive is enabled?
      • Why does the drive fault to "speed feedback"?
      • Why does the drive fault to 3 phase-fail after the drive is enabled?
      • What I can I check for a CALIBRATION FAIL trip?
      • DC590+ Encoder Feedback Card Options
      • DRV Contactor Options (955+ part numbers)
      • HOW DO I CONVERT DC590+ UK/JDE PART NUMBERS TO US PART NUMBERS?
      • What are differences between a Regen and Non-Regen 590+?
      • Why is every light on the keypad flashing on my 590+?
    • +TS8000, DSI3, & DSI8000
    • +Legacy/Discontinued VFD Products
    • What software and communication cable are used for programming?
    • DSE Lite and Drive Firmware Compatibility
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
  • +Servo Motors
  • +Step Motors
  • +Linear and Rotary Positioners
  • +Electric Cylinders
  • +T-Slot Aluminum Framing
  • +OEM Products
  • +C3 + Xpress + ETH
  • How can I stay updated on Parker electromechanical and drives product news?
  • +Legacy (Discontinued)
  • +Other

How can I make sure my DC motor does not have a problem with the Field Windings?

Revision Creation Date Revision Author
Current Revision 9 Dec 2019 6:19 PM Jack DeGrano
Revision #14 17 Oct 2019 11:30 PM Jack DeGrano
Revision #13 17 Oct 2019 11:28 PM Jack DeGrano
Revision #12 28 Aug 2019 3:25 PM Jack DeGrano
Revision #11 28 Aug 2019 3:24 PM Jack DeGrano
Revision #10 6 Aug 2019 9:06 PM Jack DeGrano
Revision #9 14 Jun 2019 4:47 PM Jack DeGrano
Revision #8 13 Jun 2019 11:51 PM Jack DeGrano
Revision #7 13 Jun 2019 11:01 PM Jack DeGrano
Revision #6 13 Jun 2019 10:56 PM Jack DeGrano
Revision #5 13 Jun 2019 10:56 PM Jack DeGrano
>
  • Compare Versions View current version
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
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
      • Mobile IoT
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
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
Parker - Engineering Your Success
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
Ā© Parker Hannifin Corp 2021