• Home
  • Investors
  • Contact Parker
  • Sign In / Register
Parker Community
  • Site
  • User
  • Site
  • Search
  • User
  • Products
  • Support
  • Divisions
  • Where to Buy
  • Careers
  • About Parker
Home Parker Community Technologies Electromechanical Group Electromechanical Knowledge Base IPA Misc - Aries Controller Replacement
Sign In / Register

Sign In

Register

  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller-
      • IPA Accessories - IPA as Ethernet/IP Scanner for Ethernet/IP I/O Adapter Devices (Video)
      • IPA Cables - P Series Motors to IPA
      • IPA Hardware - Connector Part Numbers
      • IPA Hardware - DC Power
      • IPA Hardware - Does the IPA Have Battery Backed Memory or Flash?
      • IPA Hardware - MX80L Limit/Home Wiring
      • IPA Hardware - Torque Enable Inputs Circuit (Example Wiring)
      • IPA Hardware - What is the minimum regen (braking) resistor value allowed?
      • IPA Misc - Letter of Volatility
      • IPA Misc - Absolute Encoder Compatibility (BiSS-B and BiSS-C)
      • IPA Misc - Absolute Encoder Compatibility (EnDat)
      • IPA Misc - Aries Controller Replacement
      • IPA Misc - How to Calculate Regeneration
      • IPA Misc - How to Change the IP Address
      • IPA Misc - IPA with Allen-Bradley Ethernet/IP with ETH Actuator (Video)
      • IPA Software - Add On Instructions Tutorial for Allen-Bradley Logix PLCs (Training Video)
      • IPA Software - Add-On Instructions
      • IPA Software - Analog Input Parameters, Filtering, Example Joystick Program (Video)
      • IPA Software - Assigning Limit and Home Inputs (HLBIT)
      • IPA Software - Basic Tuning using ACR-View
      • IPA Software - Change Direction of Travel (What is Positive/Negative Motion)
      • IPA Software - Communicating via ASCII over Ethernet TCP/IP
      • IPA Software - Configuration Parameter for the Feedback Type
      • IPA Software - Ethernet/IP with Allen-Bradley or Omron PLCs
      • IPA Software - Example - Ballscrew Compensation / Slope Correction
      • IPA Software - Example - Cable Winding Application
      • IPA Software - Example - Error Recovery Program
      • IPA Software - Example - Excel Spreadsheet to Upload/Download Arrays
      • IPA Software - Example - How to Home to a Hardstop
      • IPA Software - Example - Interact Xpress HMI
      • IPA Software - Example - Torque Limited Move for Clamping (with Video)
      • IPA Software - How does motion work in the ACR products (ARC7xxx, ACR9xxx, IPA, Aries-CE)
      • IPA Software - How to Change the Home Start Direction and Other Home Settings
      • IPA Software - How to Save Servo Gains
      • IPA Software - INTCAP (Position Capture)
      • IPA Software - Resetting/Setting Absolute Encoder Position and Setting Multi-Turn Range
      • IPA Software - Torque Enable Inputs Functionality
      • IPA Software - User Variables and Bits (Which are retained?)
      • IPA Troubleshooting - Endat Absolute Encoders with IPA-Feedback Errors
      • IPA Troubleshooting - ETT Actuator Noise
      • IPA Troubleshooting - PC communications (Ethernet)
      • IPA Troubleshooting - Watchdog Timeout Event Triggered or Reconnect Event Triggered Error (ACR-View)
      • IPA Troubleshooting - Why Can't I Access Parameters P0 - P4095 From My HMI or GUI?
      • z CIP Communications stop on all devices when one CIP device goes offline (copy)
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
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
  • OEM Products+
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
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
      • Mobile IoT
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Blogs
  • Forums
  • Knowledge Base
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

IPA Misc - Aries Controller Replacement

Print Friendly and PDF
Bulletin SD1429

Parker discontinued the sale of all Aries Controller (aka Aries CE) servo drives effective March 1st , 2016. The Intelligent Parker Amplifier (IPA) was designed and introduced as a replacement for the Aries Controller.  With a proven and superior product available as a replacement, Parker decided to retire the Aires CE to simplify support and to encourage customers to move to the new and better product. 

The following parts are impacted: 
AR-04CE 
AR-08CE 
AR-13CE 
All custom products based on the above products, such as:
 CP*AR-04CE-xxxxx 
CP*AR-08CE-xxxxx 
CP*AR-13CE-xxxxx

Suggested Replacements 
AR-04CE>>>IPA04-HC 
AR-08CE>>>IPA15-HC 
AR-13CE>>>IPA15-HC
 
Communications
The robust Ethernet implementation in the IPA provides outstanding performance in HMI, PC and PLC based applications. PC and HMI drives for the IPA are the same as those used with the AriesCE so that most legacy applications will communicate with the IPA without changes to the settings.
Programming 
ACR-View 6.4 and greater includes support for the IPA. Existing Aries Controller applications can be upgraded with a single button press in ACR-View. With this process, motor set-up information is updated to support new values in the IPA. AcroBasic program code developed for the Aries CE can be loaded in an IPA without modification in most applications. In some cases the faster processing of the IPA may introduce some timing changes to programs, generally reducing program complexity. 
Cables/Pin-outs 
The IPA has the same connectors and pin-outs for I/O, power, motor and motor feedback, allowing for replacement of an Aries CE without wiring changes. 

Motors and Feedback 
The IPA supports all the same motors and feedback types as the Aries controller, with the exception of the obsolete Parker smart encoders. These encoders were designated by the order code of "3E" in the MPP/MPJ series and by "Q"in all other motor families. The Parker smart encoders were 2000 line, incremental encoders that store motor set-up information in the encoder and push this data to the Aries on start-up. This data included initial hall/encoder alignment information. The IPA is not currently able to read this data or start without hall commutation. When upgrading an application that uses a smart encoder to an IPA, it will be necessary to change the motor or contact Parker about the possibility of changing the motors feedback devices via a factory based repair. 
New Features 
The IPA includes a top mounted connector housing several new features that were not present in the Aries Controller. Included are dedicated, dual inputs for disabling torque output. For convenience in replacement applications, these inputs are jumped at the factory. This connector also features analog inputs and optional 24V keep alive. 

Dimensions 
The IPA will occupy less cabinet space with a height of seven inches compared with eight for the Aries. The depth of the drives are the same and the width is similar. The mounting holes for the IPA are different than those on the Aries Controller, shifted to the left side of the drive rather than the right. The P-Clip is now more conveniently mounted on the front of the drive instead of the bottom and the mounted holes are slotted for easier install. 
jw oct 2016
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
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
      • Mobile IoT
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
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
Parker - Engineering Your Success
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
Ā© Parker Hannifin Corp 2021