Home Technologies Electromechanical Group Electromechanical Knowledge Base How to receive ASCII data
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base How to receive ASCII data
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
How to receive ASCII data

Print Friendly and PDF

The example below is an alternative the INPUT command in the ACR controller. The routine will read one ASCII character at a time from the PC or other device. To end the transmission from the third-party controller, we look for a carriage return  (ASC 13) as in  IF (ASC($V0)=13) within the ReceiveData subroutine. This can then allow the programmer to continue program execution if desired as compared to the INPUT command which inhibits program execution.

Notes: The ACR9000's USB port uses Stream1. If using Ethernet, ACR-View will connect to the first available of the 4 streams (Stream2 - 5).

To see the stream number when connected, type STREAM

Below sample uses Stream#3 while leaving ACR-View with Stream#2 connected. This will not run from ACR-View's terminal emulator. Use connect via HyperTerminal or Putty (use Port 5002 which is the ASCII port)

If testing with PBOOT within the program, use ACR-View and CLOSE #3 before doing a REBOOT command to test the power-up function.



PROGRAM
DIM LV4
DIM $V(10,50)
OPEN "STREAM3:" AS #3 : REM Open communication to PC
_loop
print #3, "enter something"
$V2="" : GOSUB ReceiveData
print #3, "something is: ",$V1
goto loop
 

_ReceiveData
$V1=""
WHILE (3)
 IF (KBHIT(3))
 $V2=GETCH(3)
 IF (ASC($V2)=13)  : rem ASC 13 is carriage return
  BREAK  : REM Break out of the WHILE loop
 ELSE
 $V1=$V1+$V2
 endif
 endif
WEND
RETURN
ENDP
 



jw 12/2016
updated 3/7/17jh
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.