• Home
  • Investors
  • Contact Parker
  • Sign In / Register
Parker Community
  • Site
  • User
  • Site
  • Search
  • User
  • Products
  • Support
  • Divisions
  • Where to Buy
  • Careers
  • About Parker
Home Parker Community Technologies Electromechanical Group Electromechanical Knowledge Base How do I implement a Fast Stop circuit on the AC10?
Sign In / Register

Sign In

Register
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
  • AC and DC Drives and Inverters-
    • AC10-
      • AC10 Heat Dissipation
      • AC10: Is the keypad detachable during operation?
      • AC10: Why am I getting over-voltage trips?
      • AC10: Why is my AC motor running hot?
      • Can I program through the keypad and DSELite on the AC10?
      • How can I configure an AC10 to run at two different speeds without using an analog input?
      • How do I connect an AC10 to a TS8000?
      • How do I clone the AC10 with the 1002-00 module?
      • How do I connect to an AC10 with the 1002-00 module as a serial converter, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and DSELite?
      • How do I connect to an AC10 using a generic RS485 device, and PDB?
      • How do I implement a Fast Stop circuit on the AC10?
      • How do I know what firmware revision my AC10 is?
      • How do I reset an AC10 back to factory defaults?
      • How do I reset the master password in an AC10?
      • How do I set up an AC10 for torque control?
      • In what type of package is the AC10 available?
      • What are the basic parameters to run an AC Induction motor from just the keypad?
      • What are the basic wiring connections of the AC10?
      • What are the environmental operating conditions for the AC10?
      • What are the minimum and maximum 3-phase input voltage ratings for the AC10?
      • What default configurations are available for the AC10?
      • What is the current overload rating for the AC10 drive?
      • What kind of I/O is available on the AC10?
      • What safety standards does the AC10 meet?
      • What software and communication cable are used for programming an AC10?
      • Why won't my AC10 run my motor?
      • Can an AC10 run a PMAC motor?
      • Updated Control Terminal Torque Specifications for AC10 VFD’s
      • Where do I get the AC10's Modbus RTU / programming connector?
    • AC30+
    • AC690+ Series+
    • AC890 Series+
    • DC590+ Series+
    • TS8000, DSI3, & DSI8000+
    • Legacy/Discontinued VFD Products+
    • What software and communication cable are used for programming?
    • DSE Lite and Drive Firmware Compatibility
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
  • Servo Motors+
  • Step Motors+
  • Linear and Rotary Positioners+
  • Electric Cylinders+
  • T-Slot Aluminum Framing+
  • OEM Products+
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
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
      • Mobile IoT
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Blogs
  • Forums
  • Knowledge Base
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

How do I implement a Fast Stop circuit on the AC10?

Print Friendly and PDF

The AC10 does not have a dedicated Safe Torque Off circuit (STO) implemented. It does have a "coast stop" functionality that can be configured.

It can also still be setup to utilize a configurable 'Fast Stop" circuit in the event the drive needs to be decelerated quickly. This FAQ covers that setup.

Required:

  • DSELite version 3.07 or greater:
  • One of the following AC10 drives:
    • AC10 IP20 drive, Frame 1 – 5, with firmware version 2.31 or greater.
    • AC10 IP20 drive, Frame 6 -12, with firmware version 3.31 or greater.
    • AC10 IP66 drive, with firmware version 4.31 or greater.

Procedure:

  1. Using DSELite configure the drive per the attached configuration example located below. Make sure to select the proper template for the AC10 frame and firmware you have.
    1. Fast Stop Example Configuration
    2. In this configuration to do a normal stop of the drive remove Digital Input DI1. To do a Fast Stop remove terminal Digital Input DI2.
  2. The connection line from the Sequencing Logic block /Running parameter, is a Feedback link. Right mouse click on the line and select "Feedback". See the picture in the appnote.
  3. Value Func 2 / Input A sets Normal decal time. Input B sets the Fast Stop time. When setting these times, there is a decimal shift, thus 0.1 = 1 seconds, 0.5 = 5 seconds.

[QuickLink for the AC10 on Parker.com] - Manual, QuickStarts, Product Support, etc

6SEP19 JD

  • safe
  • E stop
  • fast
  • off
  • emergency
  • STOP
  • AC10
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
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
      • Mobile IoT
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
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
Parker - Engineering Your Success
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
© Parker Hannifin Corp 2021