• Home
  • Investors
  • Contact Parker
  • Sign In / Register
Parker Community
  • Site
  • User
  • Site
  • Search
  • User
  • Products
  • Support
  • Divisions
  • Where to Buy
  • Careers
  • About Parker
Home Parker Community Technologies Electromechanical Group Electromechanical Knowledge Base Which Xpress Version works with my? XPR / XPR2 / XT
Sign In / Register

Sign In

Register

  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver+
    • Interact+
    • InteractX+
    • Interact Xpress-
      • How to Flashback Compact Flash (CF) Card for Parker HMIs
      • Step 3 Error when clicking Design in your PFD Project
      • Are all tags written all the time? Where to set this?
      • Auto E-Mail on Alarm activity not working with Free E-mail servers
      • Can I send an Alarm E-mail to more than one person?
      • Control Access to Panels and Tools using the Password User Levels in Xpress / Embedded Xpress (PAC)
      • How can I find out what TCP/UDP ports my software is using?
      • How do I control the Lens States for an Indicator tool in Interact Xpress?
      • How do I get through my router for remote Interact Xpress panel access?
      • How do I set a value to my device from my Xpress panel only when a button is pressed?
      • How do I write/read strings between Xpress (XPR) and ACR?
      • How to change the sort order for recipes?
      • How to switch screens from a PLC
      • How to wrap text on a tool in Xpress Manager?
      • Importing Tags into Xpress from Control Logix / Compact Logix
      • Interact Xpress Tag Rules Examples
      • Interact Xpress with Compax3 Sample for Torque Control
      • Interact Xpress with Parker-SSD AC890 Drive Products
      • InteractXpress: CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • InteractXpress: User Configurable Driver User Guide (UCON)
      • Loading Xpress Application on the XPR on bootup
      • My Xpress projects disappeared after I upgraded my Pre-2.1.6 version to 2.1.6 or higher
      • My Xpress version did not change when I did an upgrade to the latest version on my development PC
      • Not able to add tags in Tag Editor using (New Tag)
      • Step 3 Error when clicking Design in your Xpress Project
      • Test PLC driver connection setup BEFORE downloading to the HMI - If the Development PC can not talk to PLC, the HMI won't ether.
      • UCON Floating point values have Commas where the Decimal point should be
      • Updating Xpress Project versions & Creating Backup Copy
      • What size Compact Flash card is supported by XPR/XPC?
      • Where is the driver documentation and tag format information?
      • Which HMI runs Interact Xpress?
      • Which Xpress Version works with my? XPR / XPR2 / XT
      • workaround for getting flash to work on Android 4.0xxx revs
      • XPC2, XPR2 and EPX2 PowerStations no longer include audio hardware (SB975)
      • XPR/XPR2 Flashback Utilities
      • XPR/XPR2 Setting the System Time, IP address, Touchscreen Calibration require access to the Xpress Shell Screen but Application has no Exit Button
      • Xpress Manager Archive
      • Xpress Recipe Naming
      • Xpress Time and Date Tags and how they are related and used to set the HMI system Time and Date
    • IX / PCA+
    • IPX / IPC+
    • PHM / PM1 (Industrial Monitor)+
    • PA / PS / P1-P9 (DOS-based Interact HMI)+
    • PX / HPX InteractX HMIs+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • How to add images to a visualization in WebVis
    • Obsolete P1x-xxx or PMP-xxx P12-xxx or P1P-xxx or P1H-xxx ending in AR or DR and the P15 P1-10" manuals.
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
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
  • OEM Products+
  • Xpress Solutions - XPR2 + C3 + ETH+
  • Legacy+
  • Other+
  • NFI Line Filter Specification Sheets
  • How to use Motion Sizer for K series Frameless Kit motor applications
  • Technologies
    • Aerospace
    • Climate Control
    • Electromechanical Group
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

Which Xpress Version works with my? XPR / XPR2 / XT

Print Friendly and PDF

With the release of Xpress 4.x to support the new XT Widescreen format displays, there are now version restrictions based on the hardware for which you are developing or editing applications.

The XT (Widescreen) Requires Xpress 4.0 and higher. The Compact Flash memory cards that worked in the XPR/XPR2 are not compatible with the XT. The XT uses SD memory cards and requires a newer version of Embedded Windows.

The XPR/XPR2 requires Xpress 3.x and lower. Applications created and or upgraded to 4.x are not compatible with the XPR/XPR2

When opening an existing application, Xpress will ask if you want to upgrade if it is older than the version you are using to edit the files. As long as you reply NO to upgrading, the editor will open in a compatibility mode that can make changes to the old application and save changes that will work on the old units.

If you say YES to the upgrade question, it will give you a range of available versions to use.

IMPORTANT - Once upgraded, it is not possible to "Down Rev" an application. Make copies of original projects and keep the originals as backups. Upgrading goes up but never down. Downloading an older version application from your PC than the HMI has will be corrected by the HMI after the download. The first time it goes into run mode, it will take a while as it upgrades the application to the version it has running on it. If you upload the application back from the unit after it has run, the application will now be at the higher rev level of the HMI and not necessarily compatible with your development software any longer.

Xpress 4.x can not build a new application from scratch for old versions. If you need to support older versions and create applications from scratch, keep a old version application to use as a starter app. Make a copy of the starter app and then when opening it, just say no to upgrading and the editor will open in the older version mode and save your project in the old version format.

edited dom 02/13/2019

  • Xpress
  • XPR
  • XT
  • XPR2
Related
  • Technologies
    • Aerospace
    • Climate Control
    • Electromechanical Group
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • Pneumatics
    • Process Control
    • Sealing and Shielding
Parker - Global Application Links - Sidebar
  • Home
  • All Blogs
  • Home
  • Electromechanical Blog
  • Electromechanical Group Forums
  • Electromechanical Knowledge Base
  • Electromechanical Group Members
  • Mentions
  • Electromechanical Group Sub-Groups
  • Tags
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
image
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
Ā© Parker Hannifin Corp 2016