The ACR7000 family is supported by a new software tool, Parker Motion Manager (PMM). Parker Motion Manager combines the best of ACR-View and years of user feedback in a modern, user friendly and scalable software development environment. PMM is newly built and independent from ACR-View, allowing both software tools to be installed.
New Features include:
- Streamlined set-up Wizard
- Product specific status panels
- Improved terminal emulator
- New-look Oscilloscope tools
- Projects stored as single files for easy sharing and archiving
For ACR programmers new to Parker Motion Manager (PMM), many improvements have been implemented. Layout is similar in terms of having a connection, configuration wizard, program editor, status panels. This summary is a brief synopsis of major differences between the two development packages.
Parker Motion Manager software is available for ACR7000 stepper product, which is a compact 4axis stepper drive controller.
PMM will be expanded in the future to support the IPA (single axis servo drive controller) but will not support ACR9000 (multi-axis controller). The latter isn't possible as the ACR9000 had many options (usb, serial, CANopen, EthernetPowerlink) that would be too large an undertaking. A new product is in development for 9000 applications; contact your local Parker ATC distributor.
1. Both use ComACRserver which is installed with PMM or ACR-View6. If users have developed PC interfaces to the ACR9000 or IPA, these will work the same with the ACR7000.
2. When starting PMM users will immediately note Recent Projects allowing users to quickly jump in and get working. These are both on the optional Start Page and under File
Default is 9 files and can be changed.
As comparison, ACR-View had a scroll list of projects but not sorted by last used.
3. Uploading from an existing controller is now easier from the New Project window (File > New Project):
With ACR-View, users would have to create a new project, select the controller and then upload.
4. With Parker Motion Manager, projects are now stored as a single file (.pprj) making easier to transfer and share:
In ACR-View, projects were a folder with separate files for the .8k program, configuration, etc
5. In Parker Motion manager, System Code is generated every time on Finish.
In ACR-View, it was generated as users moved through the Configuration Wizard which caused issues if users re-opened the project and jumped around in the different sections to edit/tune/adjust settings.
6. Terminal window changes:
Users can now arrow up and arrow down rather than re-type commands. This much loved feature of power coders (from DOS windows of yester-year) is now available!
This is made possible as lines are now only sent when pressing enter.
A. Dedicated buttons for jumping between programs, LIST program, LIST with line numbers and Clear display.
B. Expanded buttons on the right for common commands (5 groups of 12 user buttons)
C. Expanded User buttons with multiple lines
D. The 4th and 5th group of buttons have been pre-populated with common commands.
Power users have full edit access and can re-use these groups but these pre-defined buttons help new users.
7. Defines is now in chart format making it easier for programmers to put in description for to name bits and parameters and constants.
8. PMM Windows can be docked, pinned or resized. This is a windows behavior Microsoft had expanded and evolved with .Net framework:
9. Configuration Wizard now includes Parker mechanics (actuators, precision tables and gearheads) for inches or millimeters.
This saves looking up the mechanics part numbering and catalog information to set the number of motor revs to in or mm
10. Same motor on multiple axis? Quickly populate the Configuration using Axis Copy (right-click on Axis):
10/1/19 jh
12/3/19 jh added Axis Copy