Home Technologies Electromechanical Group Electromechanical Knowledge Base PC to ACR Program Samples (Excel, LabView, VB.Net, C++, C#)
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base PC to ACR Program Samples (Excel, LabView, VB.Net, C++, C#)
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000-
        • ACR Binary Host Interface - 7000 and IPA
        • ACR7000 and IPA - AcroBasic PROGRAM SAMPLES
        • ACR7000 Connector part numbers
        • ACR7000 Controller differences to ACR9000
        • ACR74T Stepper Power Supply Sizing
        • ACR74V ACR78V: How to Reset BiSS Absolute Encoder Position
        • BE and SM Servo Motor Speed-Torque Curves at 24volts and 48volts
        • Expanded DEFINES allows numeric characters
        • Expansion I/O Information for ACR7000 and IPA
        • P Series Servo Motor Speed-Torque Curves at 24volts and 48volts
        • Parker Motion Manager Software Computer Requirements
        • Parker Motion Manager: What's New or Different Compared to ACR-View?
        • PC to ACR Program Samples (Excel, LabView, VB.Net, C++, C#)
        • Stepper Motor and Feedback Connectors
        • Time Saving Tip: Use Axis Copy if using same motor on other axes
        • Using #DEFINE inside PMM programs
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
PC to ACR Program Samples (Excel, LabView, VB.Net, C++, C#)

Print Friendly and PDF

This article is a composition of PC-based samples for ACR controllers.  Note that third-party software from Microsoft or NI is required to use these samples.

ACR_Excel_Arrays.zip Microsoft Excel sample using VBA to upload/download Arrays using ComACRServer6.
LabView Example.zip LabView2019 sample (Reading Parameters) using ComACRServer6.
LabView_with_Move_Example.zip LabView2019 sample (Read Parameters and Start Move by via IControl) using ComACRServer6.
ComACRServer6_VBNet.zip VB.Net Windows Forms sample using ComACRServer6.
ComACRServer6_CPP.zip C++ sample using ComACRServer6.
ComACRServer6_CSS.zip C# Windows Forms sample using ComACRServer6.
ComACRServer6_VB6.zip Visual Basic VB6 sample using ComACRServer6.
AcrStandaloneTerminal.zip C# Windows Presentation Foundation sample demonstrating a terminal emulator.  Also includes a feature to stream a program to an ACR line by line, ensuring the buffer is never overrun.  Useful demonstrator for CAD-to-motion applications.

 

Note the ACR communications server, ComACRserver6, is installed with Parker Motion Manager (PMM) and ACR-View.  It can also be installed separately on a PC without PMM, though it is always good to have PMM to be able to connect to the 7000 and troubleshoot.

Keywords: ACR7000, IPA, ACR9000, computer controlled, Visual Studio

  • c#
  • LABView
  • ACR
  • VBA
  • 9000
  • Visual Studio
  • IPA
  • 7000
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.