<?xml version="1.0" encoding="UTF-8" ?>
<?xml-stylesheet type="text/xsl" href="https://community.parker.com/utility/feedstylesheets/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/"><channel><title>P Series Drives - Indexer Version - Clarification of Velocity Command Switch Functionality</title><link>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2783/p-series-drives---indexer-version---clarification-of-velocity-command-switch-functionality</link><description>Frequently Asked Questions for the Electromechanical and Drives Group.</description><dc:language>en-US</dc:language><generator>Telligent Community 11</generator><item><title>P Series Drives - Indexer Version - Clarification of Velocity Command Switch Functionality</title><link>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2783/p-series-drives---indexer-version---clarification-of-velocity-command-switch-functionality</link><pubDate>Tue, 23 Feb 2021 03:18:14 GMT</pubDate><guid isPermaLink="false">0106ae23-cc79-4508-aede-1a85d082af26:8a37ff73-5184-4b46-96b3-a222aef75464</guid><dc:creator>Gannon Holt</dc:creator><comments>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2783/p-series-drives---indexer-version---clarification-of-velocity-command-switch-functionality#comments</comments><description>Current Revision posted to Electromechanical Knowledge Base by Gannon Holt on 2/23/2021 3:18:14 AM&lt;br /&gt;
&lt;p&gt;The P Series Indexer Drives (PD-04P, PD-10P, PD-35P) have a feature called Velocity Command Switch Select.&lt;/p&gt;
&lt;p&gt;This feature applies to the Velocity Mode (configured by Control Mode object 0x3000 = 2) and allows an application to either control the velocity of the motor&amp;nbsp;from the analog velocity command input (A-OVR) OR via digital inputs that will select from pre-defined velocity levels.&lt;/p&gt;
&lt;p&gt;Object 0x231A (Velocity Command Switch Select) can be configured 4 different ways.&amp;nbsp; See this table from the user guide.&lt;/p&gt;
&lt;p&gt;&lt;img alt=" " src="/resized-image/__size/480x150/__key/communityserver-wikis-components-files/00-00-00-00-10/pastedimage1614048858130v1.png" /&gt;&lt;/p&gt;
&lt;hr /&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;Set Value of 0 = velocity is only controlled by the analog command input (A-OVR), regardless of whether any digital inputs are defined as SPDx functions.&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;hr /&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;Set Value of 3 = velocity is only controlled via the inputs defined as SPD1, SPD2, and SPD3 per this table (also from the user guide)&lt;/p&gt;
&lt;p&gt;&lt;img alt=" " src="/resized-image/__size/480x350/__key/communityserver-wikis-components-files/00-00-00-00-10/pastedimage1614048979933v2.png" /&gt;&lt;/p&gt;
&lt;p&gt;Note - if there are not the correct SPDx inputs defined, the indexer will use an &amp;#39;inactive&amp;#39; for that lacking bit in the table.&amp;nbsp; (so if no SPDx inputs are defined, it will use Speed Command 1)&lt;/p&gt;
&lt;hr /&gt;
&lt;p&gt;&lt;span&gt;Set Value of 1 = allows velocity control from the SDPx inputs and your pre-defined velocity levels OR from the analog command input (A-OVR)&amp;nbsp; If both SDP1 and SDP2 are active, control will be from the analog command input (A-OVR) and not the pre-defined velocity levels.&amp;nbsp; &lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 are both inactive, then Speed Command 1 (0x2312) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is active and SPD2 is inactive, then Speed Command 2 (0x2313) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is inactive and SPD2 is active, then Speed Command 3 (0x2314) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 are both active,&amp;nbsp;then velocity is only controlled by the analog command input (A-OVR) instead of Speed Command 4 (0x2315).&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;Note - if there are not the correct SPDx inputs defined, the indexer will use an &amp;#39;inactive&amp;#39; for that lacking bit in the table.&amp;nbsp;&amp;nbsp;(so if no SPDx inputs are defined, it will use Speed Command 1)&lt;/span&gt;&lt;/p&gt;
&lt;hr /&gt;
&lt;p&gt;&lt;span&gt;Set Value of 2 = allows velocity control from the SDPx inputs and your pre-defined velocity levels OR from the analog command input (A-OVR)&amp;nbsp; If both SDP1 and SDP2 and SPD3 are active, control will be from the analog command input (A-OVR) and not the pre-defined velocity levels.&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 and SPD3 are all inactive, then Speed Command 1 (0x2312) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is active and SPD2 and SPD3 are inactive, then Speed Command 2 (0x2313) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is inactive and SPD2 is active and SPD3 is inactive, then Speed Command 3 (0x2314) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 are active and SPD3 is inactive, then Speed Command 4 (0x2315) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 are inactive and SPD3 is active, then Speed Command 5 (0x2316) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is active and SPD2 is inactive and SPD3 is active, then Speed Command 6 (0x2317) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is inactive and SPD2 and SPD3 are active, then Speed Command 7 (0x2318) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 and SPD3 are all&amp;nbsp;active,&amp;nbsp;then&amp;nbsp;velocity is only controlled by the analog command input (A-OVR) instead of Speed Command 8 (0x2319).&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;Note - if there are not the correct SPDx inputs defined, the indexer will use an &amp;#39;inactive&amp;#39; for that lacking bit in the table.&amp;nbsp;&amp;nbsp;(so if no SPDx inputs are defined, it will use Speed Command 1)&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;glh 2/2021&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;&lt;/span&gt;&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;
</description></item><item><title>P Series Drive - Indexer Version - Clarification of Velocity Command Switch Functionality</title><link>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2783/p-series-drives---indexer-version---clarification-of-velocity-command-switch-functionality/revision/2</link><pubDate>Tue, 23 Feb 2021 03:17:40 GMT</pubDate><guid isPermaLink="false">0106ae23-cc79-4508-aede-1a85d082af26:8a37ff73-5184-4b46-96b3-a222aef75464</guid><dc:creator>Gannon Holt</dc:creator><comments>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2783/p-series-drives---indexer-version---clarification-of-velocity-command-switch-functionality#comments</comments><description>Revision 2 posted to Electromechanical Knowledge Base by Gannon Holt on 2/23/2021 3:17:40 AM&lt;br /&gt;
&lt;p&gt;The P Series Indexer Drives (PD-04P, PD-10P, PD-35P) have a feature called Velocity Command Switch Select.&lt;/p&gt;
&lt;p&gt;This feature applies to the Velocity Mode (configured by Control Mode object 0x3000 = 2) and allows an application to either control the velocity of the motor&amp;nbsp;from the analog velocity command input (A-OVR) OR via digital inputs that will select from pre-defined velocity levels.&lt;/p&gt;
&lt;p&gt;Object 0x231A (Velocity Command Switch Select) can be configured 4 different ways.&amp;nbsp; See this table from the user guide.&lt;/p&gt;
&lt;p&gt;&lt;img alt=" " src="/resized-image/__size/480x150/__key/communityserver-wikis-components-files/00-00-00-00-10/pastedimage1614048858130v1.png" /&gt;&lt;/p&gt;
&lt;hr /&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;Set Value of 0 = velocity is only controlled by the analog command input (A-OVR), regardless of whether any digital inputs are defined as SPDx functions.&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;hr /&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;Set Value of 3 = velocity is only controlled via the inputs defined as SPD1, SPD2, and SPD3 per this table (also from the user guide)&lt;/p&gt;
&lt;p&gt;&lt;img alt=" " src="/resized-image/__size/480x350/__key/communityserver-wikis-components-files/00-00-00-00-10/pastedimage1614048979933v2.png" /&gt;&lt;/p&gt;
&lt;p&gt;Note - if there are not the correct SPDx inputs defined, the indexer will use an &amp;#39;inactive&amp;#39; for that lacking bit in the table.&amp;nbsp; (so if no SPDx inputs are defined, it will use Speed Command 1)&lt;/p&gt;
&lt;hr /&gt;
&lt;p&gt;&lt;span&gt;Set Value of 1 = allows velocity control from the SDPx inputs and your pre-defined velocity levels OR from the analog command input (A-OVR)&amp;nbsp; If both SDP1 and SDP2 are active, control will be from the analog command input (A-OVR) and not the pre-defined velocity levels.&amp;nbsp; &lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 are both inactive, then Speed Command 1 (0x2312) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is active and SPD2 is inactive, then Speed Command 2 (0x2313) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is inactive and SPD2 is active, then Speed Command 3 (0x2314) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 are both active,&amp;nbsp;then velocity is only controlled by the analog command input (A-OVR) instead of Speed Command 4 (0x2315).&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;Note - if there are not the correct SPDx inputs defined, the indexer will use an &amp;#39;inactive&amp;#39; for that lacking bit in the table.&amp;nbsp;&amp;nbsp;(so if no SPDx inputs are defined, it will use Speed Command 1)&lt;/span&gt;&lt;/p&gt;
&lt;hr /&gt;
&lt;p&gt;&lt;span&gt;Set Value of 2 = allows velocity control from the SDPx inputs and your pre-defined velocity levels OR from the analog command input (A-OVR)&amp;nbsp; If both SDP1 and SDP2 and SPD3 are active, control will be from the analog command input (A-OVR) and not the pre-defined velocity levels.&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 and SPD3 are all inactive, then Speed Command 1 (0x2312) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is active and SPD2 and SPD3 are inactive, then Speed Command 2 (0x2313) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is inactive and SPD2 is active and SPD3 is inactive, then Speed Command 3 (0x2314) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 are active and SPD3 is inactive, then Speed Command 4 (0x2315) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 are inactive and SPD3 is active, then Speed Command 5 (0x2316) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is active and SPD2 is inactive and SPD3 is active, then Speed Command 6 (0x2317) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is inactive and SPD2 and SPD3 are active, then Speed Command 7 (0x2318) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 and SPD3 are all&amp;nbsp;active,&amp;nbsp;then&amp;nbsp;velocity is only controlled by the analog command input (A-OVR) instead of Speed Command 8 (0x2319).&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;Note - if there are not the correct SPDx inputs defined, the indexer will use an &amp;#39;inactive&amp;#39; for that lacking bit in the table.&amp;nbsp;&amp;nbsp;(so if no SPDx inputs are defined, it will use Speed Command 1)&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;glh 2/2021&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;&lt;/span&gt;&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;
</description></item><item><title>P Series Drive - Indexer Version - Clarification of Velocity Command Switch Functionality</title><link>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2783/p-series-drives---indexer-version---clarification-of-velocity-command-switch-functionality/revision/1</link><pubDate>Tue, 23 Feb 2021 03:10:46 GMT</pubDate><guid isPermaLink="false">0106ae23-cc79-4508-aede-1a85d082af26:8a37ff73-5184-4b46-96b3-a222aef75464</guid><dc:creator>Gannon Holt</dc:creator><comments>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2783/p-series-drives---indexer-version---clarification-of-velocity-command-switch-functionality#comments</comments><description>Revision 1 posted to Electromechanical Knowledge Base by Gannon Holt on 2/23/2021 3:10:46 AM&lt;br /&gt;
&lt;p&gt;The P Series Indexer Drives (PD-04P, PD-10P, PD-35P) have a feature called Velocity Command Switch Select.&lt;/p&gt;
&lt;p&gt;This feature applies to the Velocity Mode (configured by Control Mode object 0x3000 = 2) and allows an application to either control the velocity of the motor&amp;nbsp;from the analog velocity command input (A-OVR) OR via digital inputs that will select from pre-defined velocity levels.&lt;/p&gt;
&lt;p&gt;Object 0x231A (Velocity Command Switch Select) can be configured 4 different ways.&amp;nbsp; See this table from the user guide.&lt;/p&gt;
&lt;p&gt;&lt;img alt=" " src="/resized-image/__size/480x150/__key/communityserver-wikis-components-files/00-00-00-00-10/pastedimage1614048858130v1.png" /&gt;&lt;/p&gt;
&lt;hr /&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;Set Value of 0 = only controlled by the analog command input (A-OVR), regarding of whether any digital inputs are defined as SPDx functions.&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;hr /&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;Set Value of 3 = only controlled via the inputs defines as SPD1, SPD2, and SPD3 per this table (also from the user guide)&lt;/p&gt;
&lt;p&gt;&lt;img alt=" " src="/resized-image/__size/480x350/__key/communityserver-wikis-components-files/00-00-00-00-10/pastedimage1614048979933v2.png" /&gt;&lt;/p&gt;
&lt;hr /&gt;
&lt;p&gt;&lt;span&gt;Set Value of 1 = allows velocity control from the SDPx inputs and your pre-defined velocity levels OR from the analog command input (A-OVR)&amp;nbsp; If both SDP1 and SDP2 are active, control will be from the analog command input (A-OVR) and not the pre-defined velocity levels.&amp;nbsp; &lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 are both inactive, then Speed Command 1 (0x2312) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is active and SPD2 is inactive, then Speed Command 2 (0x2313) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is inactive and SPD2 is active, then Speed Command 3 (0x2314) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 are both active,&amp;nbsp;then velocity is only controlled by the analog command input (A-OVR) instead of Speed Command 4 (0x2315).&lt;/span&gt;&lt;/p&gt;
&lt;hr /&gt;
&lt;p&gt;&lt;span&gt;Set Value of 2 = allows velocity control from the SDPx inputs and your pre-defined velocity levels OR from the analog command input (A-OVR)&amp;nbsp; If both SDP1 and SDP2 and SPD3 are active, control will be from the analog command input (A-OVR) and not the pre-defined velocity levels.&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 and SPD3 are all inactive, then Speed Command 1 (0x2312) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is active and SPD2 and SPD3 are inactive, then Speed Command 2 (0x2313) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is inactive and SPD2 is active and SPD3 is inactive, then Speed Command 3 (0x2314) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 are active and SPD3 is inactive, then Speed Command 4 (0x2315) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 are inactive and SPD3 is active, then Speed Command 5 (0x2316) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is active and SPD2 is inactive and SPD3 is active, then Speed Command 6 (0x2317) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 is inactive and SPD2 and SPD3 are active, then Speed Command 7 (0x2318) is commanded.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;/p&gt;
&lt;p style="padding-left:30px;"&gt;&lt;span&gt;If SPD1 and SPD2 and SPD3 are all&amp;nbsp;active,&amp;nbsp;then&amp;nbsp;velocity is only controlled by the analog command input (A-OVR) instead of Speed Command 8 (0x2319).&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;glh 2/2021&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;&lt;/span&gt;&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;
</description></item></channel></rss>