<?xml version="1.0" encoding="UTF-8" ?>
<?xml-stylesheet type="text/xsl" href="https://community.parker.com/utility/feedstylesheets/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/"><channel><title>Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)</title><link>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2867/replacement-keypad-part-numbers-590-690-890-ac30-ac10</link><description>Frequently Asked Questions for the Electromechanical and Drives Group.</description><dc:language>en-US</dc:language><generator>Telligent Community 11</generator><item><title>Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)</title><link>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2867/replacement-keypad-part-numbers-590-690-890-ac30-ac10</link><pubDate>Thu, 17 Jun 2021 22:55:14 GMT</pubDate><guid isPermaLink="false">0106ae23-cc79-4508-aede-1a85d082af26:80672a3f-d908-4d63-af45-1c54e3bb254d</guid><dc:creator>Daniel Cliffe</dc:creator><comments>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2867/replacement-keypad-part-numbers-590-690-890-ac30-ac10#comments</comments><description>Current Revision posted to Electromechanical Knowledge Base by Daniel Cliffe on 6/17/2021 10:55:14 PM&lt;br /&gt;
&lt;p&gt;We offer the following parts for replacement needs for the 590+, 690+, 890, AC30 and AC10 products.&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;h2&gt;590+, 690+ and 890 (frame E-J for 890)&lt;/h2&gt;
&lt;p&gt;&lt;strong&gt;6901/00/G&lt;/strong&gt;&lt;span&gt;&amp;nbsp; &amp;nbsp;=&amp;nbsp;&lt;/span&gt;Keypad replacement kit&lt;/p&gt;
&lt;p&gt;Note - I&lt;span&gt;ncludes a replacement keypad and the 1&amp;quot; connection cable that is used when the keypad is mounted on the drive directly.&amp;nbsp; This keypad can be used with all 590+ and 690+ drives.&amp;nbsp; It can also be used with 890 drives.&amp;nbsp; The 6901/00/G can be mounted directly to 890 drives frames E-J and also to the 890PX.&amp;nbsp; It cannot be mounted to 890 drives frames B-D.&amp;nbsp; The 6901/00/G can be used with &lt;span style="text-decoration:underline;"&gt;all&lt;/span&gt; 890 drives as a remote keypad.&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;Additional Note - The previous version of the keypad replacement was 6901/00 and it was blue in color.&amp;nbsp;&amp;nbsp;&lt;span style="font-family:inherit;"&gt;The product line color scheme was updated to Parker colors and the current keypad is &amp;#39;gold&amp;#39; in color now but functionally the same as the older &amp;#39;blue&amp;#39; version, which is no longer available.&lt;/span&gt;&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;CM389812&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= 1&amp;quot; connection cable only&lt;/p&gt;
&lt;p&gt;Note - N&lt;span&gt;o keypad included.&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;6052/00/G&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= Remote Mounting Kit&lt;/p&gt;
&lt;p&gt;Note - Used to remote mount the keypad on the cabinet door or elsewhere, not directly on the drive - includes mounting hardware and 3m connection cable but does&amp;nbsp;&lt;span style="text-decoration:underline;"&gt;not&lt;/span&gt; include the keypad itself.&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;CM057375U300&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= 3 m connection cable only&lt;/p&gt;
&lt;p&gt;Note - No mounting hardware or keypad included.&lt;/p&gt;
&lt;h2&gt;890 (frame B-D)&lt;/h2&gt;
&lt;p&gt;&lt;strong&gt;6511/RS232/00&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= Keypad replacement kit&lt;/p&gt;
&lt;p&gt;Note - This keypad is the one that mounts directly to the 890 B, C and D frames, which are too small to accommodate the larger 6901/00/G.&amp;nbsp; This keypad can be mounted remotely if desired and ships with a gasket and two mounting screws for that purpose.&amp;nbsp; Cable CM057375U300 can be used to connect it to the 890.&amp;nbsp; However, for remote mounting purposes, the 6901/00/G is usually preferred because it has a full text display and more features.&lt;/p&gt;
&lt;p&gt;Note - The 1&amp;quot; cable used on the 6901/00/G is not required for this keypad.&lt;/p&gt;
&lt;h2&gt;AC30&lt;/h2&gt;
&lt;p&gt;&lt;strong&gt;7001-00-00&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= IP54 graphical keypad&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;LA501991U300&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= Keypad remote mounting kit&lt;/p&gt;
&lt;p&gt;Note - Used to mount the keypad on the cabinet door or elsewhere, not directly on the drive - includes 3 m cable and screws (nothing else required) but does not include the keypad itself.&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;7001-01-00&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= Keypad blanking cover&lt;/p&gt;
&lt;p&gt;Note - This can be used to take up the space left over if a keypad is not installed on the drive.&lt;/p&gt;
&lt;h2&gt;AC10 (IP20)&lt;/h2&gt;
&lt;p&gt;&lt;strong&gt;1001-00-00&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= Remote keypad&lt;/p&gt;
&lt;p&gt;Note - The remote keypad works for all IP20 AC10 drives (models starting with &amp;quot;10G-&amp;quot;).&amp;nbsp; It can also be&amp;nbsp;used to replace the built-in keypad for frames 6-11 as this keypad is removable.&amp;nbsp; Frames 1-5 cannot have their built-in keypad replaced because it is not removable.&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;1001-01-00&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= Extension cable (1.5 m)&lt;/p&gt;
&lt;h2&gt;AC10 (IP66)&lt;/h2&gt;
&lt;p&gt;&lt;strong&gt;1601-00-00&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= Remote keypad&lt;/p&gt;
&lt;p&gt;Note - Works for all IP66 AC10 drives (models starting with &amp;quot;16G-&amp;quot;).&amp;nbsp; It can also be used to replace the built-in keypad for all frames as this keypad is removable.&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;1601-00-00&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= Extension cable (1.5 m)&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;Pricing, availability, and ordering is available via a local distributor.&amp;nbsp; Email &lt;a href="mailto:emn.service@support.parker.com"&gt;emn.service@support.parker.com&lt;/a&gt;&amp;nbsp;with your zip code if you need a local distributor contact.&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;glh&amp;nbsp; &amp;nbsp;6/2021&lt;/p&gt;
&lt;p&gt;16JUN2021 DCLIFFE -- Expanded.&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;

&lt;div style="font-size: 90%;"&gt;Tags: 6901, 890PX, 6511, AC10, AC30, 590+, keypad, 690+, 890&lt;/div&gt;
</description></item><item><title>Replacement keypad part numbers (590+ / 690+ / 890 / AC30)</title><link>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2867/replacement-keypad-part-numbers-590-690-890-ac30-ac10/revision/3</link><pubDate>Thu, 17 Jun 2021 00:33:56 GMT</pubDate><guid isPermaLink="false">0106ae23-cc79-4508-aede-1a85d082af26:80672a3f-d908-4d63-af45-1c54e3bb254d</guid><dc:creator>Gannon Holt</dc:creator><comments>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2867/replacement-keypad-part-numbers-590-690-890-ac30-ac10#comments</comments><description>Revision 3 posted to Electromechanical Knowledge Base by Gannon Holt on 6/17/2021 12:33:56 AM&lt;br /&gt;
&lt;p&gt;We offer the following parts for replacement needs for the 590+, 690+, 890, and AC30 products (does not apply to AC10)&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;6901/00/G&lt;/strong&gt;&lt;span&gt;&amp;nbsp; &amp;nbsp;=&amp;nbsp;&lt;/span&gt;Keypad replacement kit&amp;nbsp;&lt;/p&gt;
&lt;p&gt;Note - i&lt;span&gt;ncludes a replacement keypad and the 1&amp;quot; connection cable that is used when the keypad is mounted on the drive directly&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;CM389812&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= 1&amp;quot; connection cable only&amp;nbsp;&lt;/p&gt;
&lt;p&gt;Note -&amp;nbsp;&lt;span&gt;no keypad included&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;6052/00/G&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= Remote Mounting Kit&lt;/p&gt;
&lt;p&gt;Note - used to remote mount the keypad on the cabinet door or elsewhere, not directly on the drive - includes mounting hardware and 3m connection cable but does&amp;nbsp;&lt;span style="text-decoration:underline;"&gt;not&lt;/span&gt; include the keypad itself&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;CM057375U300&lt;/strong&gt;&amp;nbsp; &amp;nbsp;=&amp;nbsp; 3m connection cable only&lt;/p&gt;
&lt;p&gt;Note - no mounting hardware or keypad included&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;Pricing, availability, and ordering is available via a local distributor.&amp;nbsp; Email &lt;a href="mailto:emn.service@support.parker.com"&gt;emn.service@support.parker.com&lt;/a&gt;&amp;nbsp;with your zip code if you need a local distributor contact.&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;Additional note - the previous version of the keypad replacement was 6901/00 and it was blue in color.&amp;nbsp;&amp;nbsp;&lt;/span&gt;&lt;span style="font-family:inherit;"&gt;The product line color scheme was updated to Parker colors and the current keypad is &amp;#39;gold&amp;#39; in color now but functionally the same as the older &amp;#39;blue&amp;#39; version, which is no longer available.&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;glh&amp;nbsp; &amp;nbsp;6/2021&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;
</description></item><item><title>Replacement keypad part numbers (590+ / 690+ / 890 / AC30)</title><link>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2867/replacement-keypad-part-numbers-590-690-890-ac30-ac10/revision/2</link><pubDate>Thu, 17 Jun 2021 00:31:14 GMT</pubDate><guid isPermaLink="false">0106ae23-cc79-4508-aede-1a85d082af26:80672a3f-d908-4d63-af45-1c54e3bb254d</guid><dc:creator>Gannon Holt</dc:creator><comments>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2867/replacement-keypad-part-numbers-590-690-890-ac30-ac10#comments</comments><description>Revision 2 posted to Electromechanical Knowledge Base by Gannon Holt on 6/17/2021 12:31:14 AM&lt;br /&gt;
&lt;p&gt;We offer the following parts for replacement needs for the 590+, 690+, 890, and AC30 products (does not apply to AC10)&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;6901/00/G&lt;/strong&gt;&lt;span&gt;&amp;nbsp; &amp;nbsp;=&amp;nbsp;&lt;/span&gt;Keypad replacement kit&amp;nbsp;&lt;/p&gt;
&lt;p&gt;Note - i&lt;span&gt;ncludes a replacement keypad and the 1&amp;quot; connection cable that is used when the keypad is mounted on the drive directly&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;CM389812&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= 1&amp;quot; connection cable only&amp;nbsp;&lt;/p&gt;
&lt;p&gt;Note -&amp;nbsp;&lt;span&gt;no keypad included&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;6052/00/G&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= Remote Mounting Kit&lt;/p&gt;
&lt;p&gt;Note - used to remote mount the keypad on the cabinet door or elsewhere, not directly on the drive - includes mounting hardware and 3m connection cable but does&amp;nbsp;&lt;span style="text-decoration:underline;"&gt;not&lt;/span&gt; include the keypad itself&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;CM057375U300&lt;/strong&gt;&amp;nbsp; &amp;nbsp;=&amp;nbsp; 3m connection cable only&lt;/p&gt;
&lt;p&gt;Note - no mounting hardware or keypad included&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;Pricing, availability, and ordering is available via a local distributor.&amp;nbsp; Email &lt;a href="mailto:emn.service@support.parker.com"&gt;emn.service@support.parker.com&lt;/a&gt;&amp;nbsp;with your zip code if you need a local distributor contact.&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;Additional note - the previous version of the keypad replacement was 6901/00 and it was blue in color.&amp;nbsp; &lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;span&gt;The product line color scheme was updated to Parker colors and the current keypad is &amp;#39;gold&amp;#39; in color now but functionally the same as the older &amp;#39;blue&amp;#39; version, which is no longer available.&lt;/span&gt;&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;glh&amp;nbsp; &amp;nbsp;6/2021&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;
</description></item><item><title>Replacement keypad part numbers (590+ / 690+ / 890 / AC30)</title><link>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2867/replacement-keypad-part-numbers-590-690-890-ac30-ac10/revision/1</link><pubDate>Thu, 17 Jun 2021 00:27:15 GMT</pubDate><guid isPermaLink="false">0106ae23-cc79-4508-aede-1a85d082af26:80672a3f-d908-4d63-af45-1c54e3bb254d</guid><dc:creator>Gannon Holt</dc:creator><comments>https://community.parker.com/technologies/electromechanical-group/w/electromechanical-knowledge-base/2867/replacement-keypad-part-numbers-590-690-890-ac30-ac10#comments</comments><description>Revision 1 posted to Electromechanical Knowledge Base by Gannon Holt on 6/17/2021 12:27:15 AM&lt;br /&gt;
&lt;p&gt;We offer the following parts for replacement needs for the 590+, 690+, 890, and AC30 products (does not apply to AC10)&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;6901/00/G&lt;/strong&gt;&lt;span&gt;&amp;nbsp; &amp;nbsp;=&amp;nbsp;&lt;/span&gt;Keypad replacement kit (includes a replacement keypad and the 1&amp;quot; connection cable used when the keypad is mounted on the drive directly):&lt;/p&gt;
&lt;p&gt;Note - previous version was 6901/00 which was blue in color.&amp;nbsp; The product line color scheme was updated to Parker colors and the current keypad is &amp;#39;gold&amp;#39; in color now but functionally the same as the older &amp;#39;blue&amp;#39; version.&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;CM389812&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= 1&amp;quot; connection cable only (no keypad included)&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;6052/00/G&lt;/strong&gt;&amp;nbsp; &amp;nbsp;= Remote Mounting Kit (to remote mount the keypad on the cabinet door or elsewhere, not directly on the drive - includes mounting hardware and 3m connection cable but does&amp;nbsp;&lt;span style="text-decoration:underline;"&gt;not&lt;/span&gt; include the keypad itself)&lt;/p&gt;
&lt;p&gt;&lt;strong&gt;CM057375U300&lt;/strong&gt;&amp;nbsp; &amp;nbsp;=&amp;nbsp; 3m connection cable only (not mounting hardware or keypad included)&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;Pricing, availability, and ordering is available via a local distributor.&amp;nbsp; Email &lt;a href="mailto:emn.service@support.parker.com"&gt;emn.service@support.parker.com&lt;/a&gt;&amp;nbsp;with your zip code if you need a local distributor contact.&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;&lt;/p&gt;
&lt;p&gt;glh&amp;nbsp; &amp;nbsp;6/2021&lt;/p&gt;
&lt;div style="clear:both;"&gt;&lt;/div&gt;
</description></item></channel></rss>