Home Technologies Electromechanical Group Electromechanical Knowledge Base 590+ - Transferring a Configuration to a Drive with a Different Power Level
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base 590+ - Transferring a Configuration to a Drive with a Different Power Level
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
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
  • AC and DC Drives and Inverters-
    • AC10+
    • AC30+
    • AC690+ Series+
    • AC890 Series+
    • DC590+ Series-
      • How do I start troubleshooting a 590+?
      • What are the basic wiring connections required to run a motor, using the factory default drive?
      • How to Extract and Install Parameters to the 590+ Drive using DSE Lite
      • Why won't my motor run?
      • How can I make sure my DC motor does not have a problem with the Field Windings?
      • Why is my DC motor running hot?
      • 590+: Is the keypad detachable during operation?
      • Can I disable the field to run Brushed PMDC (Permanent Magnet DC motor) on a 590+?
      • Can I select between Manual Speed Reference and Line Speed Trim Setting for the same Analog Input?
      • Can you download a DSELite file into the drive when the drive is running?
      • How can I get the DSELite software the 590+ uses?
      • How can I make sure the motor will not start rotating until the speed pot is at 0?
      • How can I manually tune a 590+ drive to my motor?
      • How can I pre-trip "speed feedback" alarm before the drive trips?
      • How can I replace the control boards in 590+ Frame 1 and Frame 2 drives?
      • How can I set up a 590+ to be a field controller?
      • How can I upgrade a 590+ Frame 1 or 2 drive version 5.x or 7.x to version 8.x - Control Board and Configuration
      • How can the 590+ be programmed?
      • How can the drive configuration be reset to factory defaults?
      • How do I clone my 590+ Drive with the keypad?
      • How do I copy the configuration of one drive to another using the keypad?
      • How do I flash my 590+ drive to a newer Minor Revision of Firmware?
      • How do I know what firmware revision my 590+ is?
      • How do I set up a 590+ External Stack?
      • How to I configure the 590+ for Preset Speeds?
      • Is there anything I can check for a SEQ PRE READY alarm?
      • Modbus TCP/IP Addressing for the 590+ drive with the Ethernet Techbox
      • My DC590+ drive is displaying a Missing Pulse Alarm, what should I do?
      • The 590+ is enabled, but the main contactor doesn't close. Why?
      • Upgrading a control door from a 590 to a 590+
      • What accessories can be added to the 590+?
      • What analog and digital I/O is available on the 590+?
      • What are the Communication options for the 590+?
      • What are the communication settings for the 590+ for the P3 Port?
      • What are the differences between the 590 and 590+?
      • What are the minimum and maximum 3phase input ratings for the 590+?
      • What are the reference power supplies available to terminal connections on the 590+?
      • What are the types of Speed Feedback for the 590+?
      • What is the current overload rating for the 590+ drive?
      • What is the maximum operating altitude for the 590+?
      • What is the operating temperature for the 590+?
      • What safety standards does the 590+ meet?
      • What USB-serial adapter should I use?
      • Why does the drive fault to "Over-Voltage" after the drive is enabled?
      • Why does the drive fault to "speed feedback"?
      • Why does the drive fault to 3 phase-fail after the drive is enabled?
      • What I can I check for a CALIBRATION FAIL trip?
      • 590+ - Transferring a Configuration to a Drive with a Different Power Level
      • 598/599+ Stack Controller Replacements
      • DC590+ Encoder Feedback Card Options
      • DRV Contactor Options (955+ part numbers)
      • HOW DO I CONVERT DC590+ UK/JDE PART NUMBERS TO US PART NUMBERS?
      • Speed Regulation with 590+ Drives
      • Troubleshooting a DC brushed motor
      • What are differences between a Regen and Non-Regen 590+?
      • What does "NET FAIL" indicate in DSE Lite when using a LinkNet Techbox module on my 590+ drive?
      • Why is every light on the keypad flashing on my 590+?
    • TS8000, DSI3, & DSI8000+
    • Legacy/Discontinued VFD Products+
    • What software and communication cable are used for programming?
    • DSE Lite and Drive Firmware Compatibility
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
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
590+ - Transferring a Configuration to a Drive with a Different Power Level

Print Friendly and PDF

In the event a 590+ (or 955+) needs to be replaced, it is sometimes necessary to use a model with a different power rating due to availability constraints. However, using a unit with a different power level means that it will not be possible to transfer the configuration via the keypad. It is also not possible to transfer the configuration using a Full Install in DSE Lite because this will overwrite the drive’s PCODE, an internal parameter that configures the drive’s power level.

The correct procedure for transferring a configuration from one 590+/955+ to another one with a different power level is explained in this article. Required materials are:

  • A copy of DSE Lite, freely available here: DSE Lite
  • A 590+ programming cable, part number CM351909. This can be ordered from a Parker distributor.
  • A USB-RS232 converter with an FTDI chipset. Parker does not sell these, but they are available from many cable and electronics vendors online.

This procedure assumes a backup file of the configuration already exists. If not, the article here will explain how to extract a working backup copy:

How to Extract and Install Parameters to the 590+ Drive using DSE Lite

Installing the Configuration

  1. Connect to the new 590+ using the same method used to connect to the old one.
  2. Click Command > Install (do not do a Full Install) and wait for the installation to finish.
  3. Make a record of all the drive parameters shown in MAGENTA. These are frame-dependent parameters and will need to be entered manually. These can be found on page 1 and page 2 in the configuration file. An easy way to record these is to print the configuration to PDF or paper.
  4. Click Command > Extract Drive Parameters and wait for the extraction to finish.
  5. Manually reenter each frame-dependent parameter in DSE Lite. Values that already match can be skipped.
  6. Click Command > Full Install and wait for the installation to finish.
  7. Run an armature current loop autotune (DO NOT run a field autotune). This can be done from the keypad. The motor shaft does not need to be disconnected from the load for this. The procedure for an armature current loop autotune can be found in the manual here: 590+ V8 DRV Manual, page 4-8
  8. After performing a Save Parameters from the keypad, reconnect DSE Lite and click Command > Extract Drive Parameters. Click File > Save and save this configuration to the PC as a backup.

16DEC2021 DCLIFFE

  • pcode
  • Install
  • 955+
  • Extract
  • 590+
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.